Accelerate 5G FWA Device Test

White Paper

Fixed-location services, also known as fixed wireless access (FWA), are a rapidly growing market. Fixedlocation devices are typically used to provide access to fast data connections in areas where broadband services are not yet available and not easily deployed.

Because Wi-Fi is widely available, many fixed-location devices access broadband with an over-the-air connection to fourth- or fifth-generation cellular technology (4G or 5G) as defined by the 3rd Generation Partnership Project (3GPP), then convert to wireless local area network (WLAN) for use within a region, building, or home