此页面暂时不提供中文版本。我们计划在不久的将来提供更多内容并支持中文。
Imagine you're troubleshooting a high-speed digital circuit, and every signal detail matters. You connect a passive probe to your oscilloscope, but the signal appears distorted, with unexpected noise creeping in.
The issue isn't with your circuit — it's with your probe. In high-frequency applications, passive probes can introduce loading effects that alter the signal you're trying to measure.
This is where active probes come in. Designed to handle high-speed, low-voltage signals without degrading their integrity, active probes are essential tools for capturing accurate measurements in demanding scenarios. But what makes these probes so effective, and when should you use them?
Understanding Active Probes
Active probes are a type of oscilloscope probe that incorporate active electronic components, such as transistors or amplifiers, right at the probe tip.
These components help maintain signal integrity, especially when working with high-frequency signals or low-voltage measurements.
Unlike passive probes, active probes are designed to offer a high input impedance and low capacitance, minimizing the loading effect on the circuit under test.
| Key Takeaway |
|---|
| Active probes offer enhanced accuracy for high-frequency and sensitive measurements by reducing signal distortion and minimizing the impact on the circuit under test. They are vital for engineers who need precise data in complex and demanding applications. |
Key Features of Active Probes
Active probes have several characteristics that set them apart from other types of probes:
- High bandwidth: Active probes typically offer a higher bandwidth than passive probes, often reaching several gigahertz. This is crucial when working with high-speed digital signals or RF applications.
- High input impedance: Active probes maintain a high input impedance across a wide frequency range, reducing the risk of loading effects that can distort the signal you’re measuring.
- Low input capacitance: These probes feature low input capacitance, which helps minimize the impact on the circuit's behavior. This is particularly important in high-frequency measurements where capacitance can affect signal integrity.
- Integrated amplification: With built-in amplification, active probes can provide better signal strength, ensuring weak signals are measured accurately.
- Differential measurement capabilities: Many active probes support differential measurements, allowing you to measure the voltage difference between two points without a direct connection to the ground.
Why Use Active Probes?
Choosing the right probe for your measurement needs is crucial, especially in environments where signal integrity is vital. Here’s why you might opt for an active probe:
1. High-Frequency Measurements
Active probes are ideal for high-frequency measurements where passive probes may not provide accurate results due to their limited bandwidth and higher capacitance. The higher bandwidth allows you to capture and analyze fast signals with minimal distortion.
2. Low-Voltage Signals
When measuring low-voltage signals, passive probes can introduce significant noise or fail to pick up the signal altogether. Active probes, with their integrated amplification, offer better sensitivity for these delicate measurements, ensuring accurate data capture.
3. Minimizing Circuit Loading
The high input impedance and low capacitance of active probes minimize their impact on the circuit being tested. This is especially important when dealing with sensitive analog circuits, where even a small amount of additional load can alter the behavior of the circuit.
4. Differential Measurements
Active probes are designed to handle differential measurements, making them useful for analyzing differential signals in balanced circuits or situations where ground loops could affect measurement accuracy.
Upgrade Your Lab, not Your Budget
Types of Active Probes
Active probes come in several varieties, each designed for specific applications:
- Single-ended active probes: Single-ended active probes are designed to measure the voltage at a single point relative to a common ground. They are ideal for applications where a direct ground connection is available, and you only need to measure one point in the circuit.
- Differential active probes: Differential active probes measure the voltage difference between two points, allowing you to measure signals without a common ground reference. They are particularly useful in applications like high-speed data buses, differential pairs in communication protocols, or RF circuits.
- High voltage active probes: These probes are specifically designed for measuring high-voltage signals while providing high input impedance and isolation from the circuit under test. They are used in power electronics, automotive electronics, and other applications where high-voltage measurements are required.
How to Choose the Right Active Probe
Selecting the right active probe involves considering several factors:
- Frequency range and bandwidth: Match the probe’s bandwidth to your signal frequency to ensure accurate measurements. As a rule of thumb, choose a probe with a bandwidth at least five times higher than the highest frequency component of your signal.
- Input impedance and capacitance: For high-frequency signals, select a probe with high input impedance and low capacitance to avoid loading effects.
- Probe tip accessories: Consider the types of accessories available for the probe, such as fine tips for SMD components, ground leads, and adapters for different types of connectors.
- Compatibility with oscilloscope: Ensure that the probe is compatible with your oscilloscope’s input and measurement capabilities. Some oscilloscopes may require a specific type of probe or a specific impedance matching.
- Voltage rating: Make sure the probe can handle the voltage levels present in your application, especially if you are working with high-voltage circuits.
Comparison of Active vs. Passive Probes
| Feature | Active Probes | Passive Probes |
|---|---|---|
| Bandwidth | High (up to several GHz) | Limited (typically up to 500 MHz) |
| Input Impedance | High (typically 1 MΩ or more) | Varies (commonly 10 MΩ) |
| Input Capacitance | Low (typically a few pF) | Higher (typically 10-20 pF) |
| Signal Amplification | Yes | No |
| Differential Measurements | Supported | Not typically supported |
| Application Suitability | High-frequency, low-voltage, RF | General-purpose, low-frequency |
| Cost | Higher | Lower |
Best Practices for Using Active Probes
To get the most out of your active probes and ensure accurate measurements, consider these best practices:
- Calibrate the probe: Regular calibration maintains the accuracy of your measurements. Different active probes may require specific calibration procedures to align their performance with the oscilloscope. Always follow the manufacturer’s guidelines for calibration intervals and methods to avoid drift and inaccuracies.
- Use proper grounding: Grounding is vital to reduce noise and prevent ground loops that can interfere with signal integrity. Always use the shortest possible ground connection to minimize inductance, and avoid large ground loops by connecting the ground as close to the measurement point as possible. Using dedicated grounding accessories, like short ground springs, can further help reduce interference.
- Match the probe to the application: Select the probe that best fits your specific measurement needs. Consider factors such as signal frequency, voltage level, circuit type, and whether you require single-ended or differential measurements. Using a probe outside its intended range can lead to measurement errors, signal distortion, or even damage to the probe or equipment.
- Minimize probe loading: To minimize the impact of the probe on your circuit, choose a probe with a high input impedance and low input capacitance, especially for high-frequency or sensitive analog measurements. Keep the probe cables as short as possible to reduce parasitic capacitance and inductance, which can alter the behavior of the circuit under test.
- Optimize probe placement: Position the probe carefully to avoid picking up noise or interference. When probing high-speed digital signals or RF circuits, keep the probe tip close to the test point and minimize the loop area between the probe tip and ground. This reduces the risk of picking up unwanted noise or electromagnetic interference.
- Regular maintenance and inspection: Regularly inspect the probe for any signs of wear and tear, especially at the tip, cable, and connectors. Damaged or worn-out probe tips can lead to poor contact, increased noise, or unreliable measurements. Clean the probe tips and connectors with appropriate cleaning materials to maintain good electrical contact and signal integrity.
- Store probes properly: When not in use, store your active probes in protective cases or holders to prevent physical damage and contamination. Avoid exposing them to extreme temperatures, humidity, or mechanical stress that could degrade their performance over time.
- Use appropriate accessories: Use the right accessories, such as fine probe tips, micro-grabbers, and ground springs, to suit the specific measurement task. These accessories can help improve signal fidelity and provide a stable connection to small or delicate components.
Following these best practices will ensure your active probes deliver consistent and reliable measurements, prolonging their lifespan and maintaining the integrity of your testing processes.
Conclusion
Active probes offer the precision and reliability needed for accurate measurements in high-frequency and low-voltage applications. They reduce signal distortion, minimize loading effects, and support differential measurements, making them an essential tool for any engineer working with complex circuits.
If you're looking to equip your lab with high-quality instruments at a lower cost, check out the Keysight Used Equipment Store. You’ll find certified pre-owned oscilloscopes, spectrum analyzers, function generators, and multimeters that deliver premium performance without the premium price tag — all with fast shipping and guaranteed reliability.

Whenever You’re Ready, Here Are 5 Ways We Can Help You
- Browse our Premium Used Oscilloscopes.
- Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri - Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
- Create an account to get price alerts and access to exclusive waitlists.
- Talk to your account manager about your specific needs.
Subscribe to Get Our Latest News, Updates, and Articles.
Get Email Updates