Oscilloscope Glossary
What Is Resistance Measured In?
Introduction
Resistance is measured in ohms (symbol Ω), the SI unit equal to one volt per ampere. In an incandescent lightbulb, electrical resistance causes the filament to heat up until it glows and produces light. This guide explains resistance units, how to measure resistance, and why impedance becomes important at higher frequencies.
When measuring resistance, even the test leads can affect your reading. The connection method you choose determines whether that extra resistance becomes part of the measurement.
Overview
- The unit: The ohm (Ω) is one volt per ampere. Ohm's law links the three quantities: V = IR.
- The scale: Resistance values range from micro-ohms to gigaohms, covering applications from busbar connections to cable insulation.
- The instruments: A multimeter measures resistance directly, while a micro-ohm meter is designed for very low resistance measurements.
- The limit: Resistance alone does not describe how a component behaves at higher frequencies. Impedance includes both resistance and reactance and can be measured using a network analyzer or impedance analyzer. The Keysight E5071C, available used, supports measurements up to 20 GHz with options 2K5 or 4K5. Its data sheet lists May 31, 2021, as the last order date, and Keysight recommends the E5080B for new purchases.
What Is Electrical Resistance?
Resistance is an object's opposition to the flow of electric current. In metal conductors, resistance results from interactions between moving electrons and the material's atoms. For a given voltage, a higher resistance means a lower current.
Resistance and Ohm's Law
Ohm's law is named after the German physicist Georg Simon Ohm, who published it in 1827. It describes the relationship between resistance, voltage (electrical potential difference), and current. The law can be written in 3 ways:
- Voltage equals current times resistance (V = IR)
- Current equals voltage divided by resistance (I = V/R)
- Resistance equals voltage divided by current (R = V/I)
The reciprocal of resistance is conductance, G = 1/R, measured in siemens (S); see the conductance formula. For a quick calculation, use the Ohm's law calculator, or read the longer explanation in What Is Ohm's Law?.
Key Takeaway
Resistance limits current. A multimeter measures it directly, while in AC and RF circuits, resistance is the real component of impedance.
What Is Resistance Measured In? The Ohm
Named after Georg Ohm, the ohm (Ω) is the standard unit of electrical resistance. A 10 V supply across a 5 Ω resistor drives 2 A, because I = V/R = 10 V / 5 Ω, consistent with the National Institute of Standards and Technology (NIST) definition of one ohm as one volt per ampere.
Sub-Units and Multiples of the Ohm
Resistance spans a wide range, so engineers use SI prefixes such as:
- Micro-ohm (µΩ) = 1/1,000,000 of an ohm
- Milliohm (mΩ) = 1/1,000 of an ohm
- Kiloohm (kΩ) = 1,000 ohms
- Megohm (MΩ) = 1,000,000 ohms
- Gigaohm (GΩ) = 1,000,000,000 ohms
A 4.7 kΩ resistor is 4,700 Ω. Connector contact resistance is usually quoted in milliohms, and cable insulation resistance in megohms or gigaohms.

How Is Resistance Measured?
The usual tool is the ohmmeter, which is built into most multimeters. A multimeter handles most everyday resistance measurements. For specialized applications, the guide to instruments for measuring resistance compares multimeters with bridges, LCR meters and micro-ohm meters. For the steps on a single part, see how to test a resistor with a multimeter.
How Does an Ohmmeter Work?
A digital multimeter sends a small, known test current through the part and measures the voltage across it. It then applies Ohm's law, R = V/I, to display the resistance. Keysight's technical support article on resistance measurement explains that the test current can heat the component and affect its resistance. This is particularly important for temperature-sensitive components, as Keysight's DMM guidance notes. Switch off the circuit, discharge any capacitors and, where you can, disconnect the part before measuring, as Keysight's guide to testing a resistor advises.
The connection method also affects measurement accuracy. Two common approaches are:
- Two-wire: The same pair of leads carries the current and senses the voltage, so the lead resistance is included in the reading. That suits resistances well above the leads' own.
- Four-wire (Kelvin): One pair of leads carries the test current, while a separate pair measures the voltage directly across the component, minimizing errors caused by lead resistance. Keysight's resistor-testing guide says it removes lead-wire resistance errors, which matters most for low-value resistors.
For very low resistance values, a dedicated instrument can help. According to its data sheet, the Keysight 34420A, pictured above, offers resistance sensitivity down to 100 nΩ and supports both 2-wire and 4-wire measurements.
Can an Oscilloscope Measure Resistance?
Oscilloscopes display how electrical signals change over time. They measure voltage rather than resistance directly. With a current probe, or a shunt resistor of known value, they can show current as well. For a component behaving as a pure resistance, dividing the voltage across it by the current through it gives its resistance, provided the current is not zero. This can help you observe resistance changes during operation, such as when a thermistor heats up. For a single fixed part, a multimeter is simpler.
How Does Resistance Affect Signal Integrity?
Resistance affects signal quality in high-speed digital circuits by contributing to signal loss as current travels through conductors. At radio frequencies, the skin effect causes current to concentrate near the surface of a conductor, as explained by HyperPhysics. Attenuation, the drop in signal amplitude along a wire or line, reduces the signal that reaches the receiver. Along with the effects of capacitance and inductance, resistance contributes to a signal path's impedance. Proper impedance matching helps reduce signal reflections.
Where Does Resistance Become Impedance?
In an ideal DC circuit, resistance describes the opposition to current. In AC and RF circuits, impedance includes both resistance and reactance, which comes from inductance and capacitance. Impedance (Z = R + jX) is also measured in ohms. A physical resistor also has small amounts of parasitic inductance and capacitance, so its impedance can differ from its DC resistance as frequency increases.

A network analyzer measures reflection (S11) across a frequency sweep and can calculate impedance from those measurements. An LCR meter can also measure impedance, typically at lower frequencies. For more detail, see how to measure impedance for measurement methods and instruments, or the impedance formula guide for the calculations.
Why Does Understanding Resistance Matter?
The table shows how resistance affects current and power dissipation under different conditions:
| Factor | High Resistance | Low Resistance |
|---|---|---|
| Current Flow | Decreased | Increased |
| Power Dissipated (same voltage) | Decreased | Increased |
| Power Dissipated (same current) | Increased | Decreased |
Decreased
Increased
Decreased
Increased
Increased
Decreased
The power comparisons differ because one assumes constant voltage and the other assumes constant current. At a fixed voltage, a lower resistance results in greater power dissipation. At a fixed current, a higher resistance results in greater power dissipation.
What Factors Influence Electrical Resistance?
Several factors influence resistance:
- Material: Different materials offer varying opposition to current flow. Copper and aluminum are used as conductors because of their low resistivity, while rubber and glass are insulators with very high resistivity.
- Cross-sectional area: A larger cross-sectional area gives the current more paths, which reduces resistance.
- Length: For a wire of the same material and thickness, a longer wire has greater resistance because resistance increases with length.
- Temperature: In most metal conductors, resistance rises with temperature. The atoms vibrate more at higher temperatures, which increases the chances of collision with the electrons.
For a uniform conductor, the first three combine in one formula, according to HyperPhysics
where ρ is the material's resistivity, L is the length and A is the cross-sectional area. Doubling the length doubles the resistance, and doubling the area halves it.
What Are the Types of Resistors?
Common types of resistors include:
- Fixed Resistors: These have a fixed value of resistance. They set a current or divide a voltage.
- Variable Resistors (Potentiometers and Rheostats): The resistance of these devices can be adjusted, which makes them useful for setting a level, as in a volume control (a potentiometer), or limiting current (a rheostat).
- Thermistors: These are temperature-sensitive resistors. Their resistance rises or falls with temperature, according to Keysight's resistor-testing guide.
- Photoresistors (Light-Dependent Resistors): Their resistance changes with the light that falls on them, as the same guide notes.
How Does Resistance Combine in Series and Parallel Circuits?
In series circuits, total resistance (R_total) is the sum of the individual resistances:
In parallel circuits, total resistance follows this formula, as shown in OpenStax College Physics:
Consider 3 resistors with values of 100 Ω, 220 Ω and 330 Ω connected in series or parallel. In series, their total resistance is 650 Ω. In parallel, the reciprocals add to 0.01 S + 0.00455 S + 0.00303 S = 0.01758 S (siemens, or 1/Ω), giving a total resistance of about 56.9 Ω, which is lower than the smallest individual resistor.
How Does Resistance Affect Power Consumption?
The amount of electrical power a component converts into heat depends on its resistance and the current flowing through it or the voltage across it.
Resistance and Joule's Law
Joule's law describes how electrical current generates heat in a resistor. The rate at which heat is produced is the electrical power, expressed as P = I²R or P = V²/R, as derived from Ohm's law in OpenStax Physics. For a given current, a higher resistance dissipates more power as heat.
A 100 Ω resistor carrying 0.1 A dissipates 1 W (P = 0.1² × 100). At 0.2 A, the same resistor dissipates 4 W, so doubling the current quadruples the heat. At 0.3 A it dissipates 9 W, nine times the power at 0.1 A.

What Does This Mean for Circuit Design?
Joule's law matters to designers for two reasons:
- Thermal Management: At a given current, a higher resistance in the current path generates more heat, which can cause components to fail.
- Intended Heating: In devices such as electric heaters, resistance is used to convert electrical energy into heat.
Key Points About Measuring Resistance
Resistance is measured in ohms, and the prefix tells you the scale. At DC, Ohm's law links resistance to voltage and current, and a multimeter is enough for most checks. Very low resistance values may require a four-wire measurement, while AC and RF measurements often require evaluating impedance rather than resistance alone. At the extreme end of resistance measurements, superconductors can have zero DC resistance below a critical temperature, as explained by OpenStax University Physics.
A multimeter covers most resistance checks.

Browse Used Oscilloscopes
An oscilloscope shows how a signal changes over time, which a single multimeter reading cannot.
Explore used network and impedance analyzers and LCR meters.
Frequently Asked Questions
No. Resistance is the property that limits current, and the ohm (Ω) is the unit it is measured in. A 10 Ω resistor has a resistance of 10 ohms.
OL typically indicates an over-range or open-circuit condition. According to Keysight's resistor-testing guide, this can mean the resistance exceeds the meter's maximum range or the test leads are not making a proper connection. Check the connections and adjust the measurement range if needed.
Whenever You’re Ready, Here Are
5 Ways We Can Help You
Browse our used oscilloscopes
Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
Contact our sales support team
Create an account to get price alerts and access to exclusive waitlists
Talk to your account manager about your specific needs
Sources
- National Institute of Standards and Technology, SI Units: Electric Current: the ohm as the SI unit of resistance, one volt per ampere.
- IEEE Engineering and Technology History Wiki, Ohm's Law: publication of the law in 1827.
- Georgia State University, HyperPhysics: Resistance and Resistivity: R = ρL/A and the skin effect at radio frequencies.
- OpenStax, College Physics 2e: Resistors in Series and Parallel: the series and parallel formulas.
- OpenStax, Physics: Electric Power: P = I²R and P = V²/R.
- OpenStax, University Physics Volume 2: Superconductors: zero DC resistance below a critical temperature.
- Keysight Technical Support, 3 Traps to Avoid When Making Resistance Measurements: the test current method and self-heating.
- Keysight Technical Support, DMM Resistance Measurement Considerations: four-wire connections and power dissipation in temperature-sensitive parts.
- Keysight Technologies, 34420A Nanovolt/Micro-Ohm Meter data sheet (5968-0161EN): 100 nΩ resistance sensitivity and 4-wire or 2-wire ohms.
- Electrical Engineering Portal, Joule's Law: the heat a current produces in a resistor.
- TechTarget, Conductor: conductors and insulators.
- Keysight Technologies, E5071C ENA Vector Network Analyzer data sheet (5989-5479EN, 2020 edition): options 2K5 and 4K5 at 300 kHz to 20 GHz, the last order date of M
- Keysight Used Equipment Store, How to Test a Resistor with a Multimeter: disconnecting the part and discharging capacitors, the OL reading, four-wire (Kelvin) connections, and thermistors and light-dependent resistors.
- Keysight Used Equipment Store, Conductance Formula: conductance as the reciprocal of resistance, measured in siemens.