G10-3o601
CVSS:
3.6 (AV:N/AC:H/Au:S/C:P/I:P/A:N)
False Positive:
f
Variants:
1
Year:
2010
Description
This strike exploits an SQL injection vulnerability in Oracle Database Server.
The vulnerability is due to input validation errors in the DROP_CHANGE_SOURCE and ALTER_CHANGE_SOURCE procedures of the DBMS_CDC_PUBLISH package.
Remote authenticated attackers with EXECUTE permission on the SYS.DBMS_CDC_PUBLISH package can exploit this vulnerability by sending a specially crafted parameter to the affected procedures.
Successful exploitation would result in disclosure of information, and modification or manipulation of the data in the underlying database.
CVE
References
http://secunia.com/advisories/39438