Keysight Advances Quantum Engineering with New System-Level Simulation Solution 

Quantum System Analysis reduces reliance on costly cryogenic testing and accelerates validation of superconducting quantum systems 

SANTA ROSA, Calif. OCTOBER 29, 2025

Keysight Technologies, Inc. (NYSE: KEYS) today announced the release of Quantum System Analysis, a breakthrough Electronic Design Automation (EDA) solution that enables quantum engineers to simulate and optimize quantum systems at the system level. This new capability marks a significant expansion of Keysight’s Quantum EDA portfolio, which includes Quantum Layout, QuantumPro EM, and Quantum Circuit Simulation. This announcement comes at a pivotal moment for the field, especially following the 2025 Nobel Prize in Physics, which recognized advances in superconducting quantum circuits—a core area of focus for Keysight’s new solution.

System-level quantum analysis has long been a challenge due to the complexity of integrating diverse physical domains—electromagnetic, circuit, and quantum dynamics—into a unified simulation environment. Traditional approaches often rely on fragmented tools and repeated cryogenic experiments, which are both time-consuming and costly. Keysight’s Quantum System Analysis bridges this gap by providing a cohesive platform that enables early validation of quantum system designs, reducing development cycles and improving design confidence.

Quantum System Analysis empowers researchers to simulate the quantum workflow, from initial design stages to system-level experiments, reducing reliance on costly cryogenic testing and accelerating time-to-validation. This integrated approach supports simulations of quantum experiments and includes tools to optimize dilution fridge input lines for thermal noise and qubit temperature estimation.

Quantum System Analysis introduces two transformative features:

  • Time Dynamics Simulator: Models the time evolution of quantum systems using Hamiltonians derived from electromagnetic or circuit simulations. This enables accurate simulation of quantum experiments such as Rabi and Ramsey pulsing, helping researchers understand qubit behavior over time.
  • Dilution Fridge Input Line Designer: Allows precise modeling of cryostat input lines to qubits, enabling thermal noise analysis and effective qubit temperature estimation. By simulating the fridge’s input architecture, engineers can minimize thermal photon leakage and improve system fidelity.

Chris Mueth, Senior Director for New Markets at Keysight, said: “Quantum System Analysis marks the completion of a truly unified quantum design workflow, seamlessly connecting electromagnetic and circuit-level modeling with comprehensive system-level simulation. By bridging these domains, it eliminates the need for fragmented toolchains and repeated cryogenic testing, enabling faster innovation and greater confidence in quantum system development.”

Mohamed Hassan, Quantum Solutions Planning Lead at Keysight, said: “Quantum System Analysis is a leap forward in accelerating quantum innovation. By shifting left with simulation, we reduce the need for repeated cryogenic experiments and empower researchers to validate system-level designs earlier in the development cycle.”

Quantum System Analysis is available as part of Keysight’s Advanced Design System (ADS) 2026 platform and complements existing quantum EDA solutions. It supports superconducting qubit platforms and is extensible to other modalities such as spin qubits, making it a versatile choice for quantum R&D teams.

Resources:

About Keysight Technologies   

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product life cycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com. 

Contacts

Andrea Mueller
Americas/Europe
andrea.mueller@keysight.com

Fusako Dohi, Asia
+81 42 660–2162
fusako_dohi@keysight.com