Choose a country or area to see content specific to your location
애플리케이션 노트
Why is Temperature Profiling of Batteries Important?
Charge and discharge currents increase the temperature of batteries and temperature directly affects the lifespan and storage capacity of batteries. Batteries tend to be efficient and provide a normal life span at room temperatures. When batteries are subjected to cold temperatures, their capacity is greatly reduced and as temperatures increase above room temperature, their life span is reduced. At extreme temperatures, batteries can break down in several stages; leakage, smoke, fire and explosion. Manufacturers often perform abuse tests to determine the temperatures for each of the stages of breakdown. When batteries fail spectacularly with smoke and fire it is typically due to a short causing a rapid discharge and greatly increased heat. So newer batteries have an extra protection that acts as a fuse to avoid an external short circuit.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.