S9130A Performance 5G Multi-Band Vector Transceiver

데이터 시트

System Performance

 

Conditions

 

Information and data contained in this data sheet is subject to change without notice.

In addition to the following conditions, the S9130A system performance, documented in this data sheet, is valid for an ambient temperature of 25 °C unless otherwise noted.

• The system is within its calibration cycle.

• The system has been stored at an ambient temperature within the allowed operating range for at least two hours before being powered on.

• The system has been powered on continuously for at least 45 minutes warm-up time, with the IQ Analyzer or X-Series application (e.g. 5G NR) running, and the M1741A mmWave Transceiver powered on (verify that LEDs are on). If the system met these warm-up requirements and there is a brief power shutdown, such as a system reboot, allow 20 minutes of warm-up time after the system is powered back on.  

• The alignments have been run in order of “Align Now All”, “Align IF Cable” and “Align RRH Amplitude” for the first use, after the warm-up period.

• The “Align Now All” alignments have been run after the warm-up period:

o Within the previous 7 days

o If the PXIe subsystem internal temperature has changed more than 5°C from the previous “Align Now All” alignments

• The alignments have been run in order of “Align Now All”, “Align IF Cable” and “Align RRH Amplitude”, after the warm-up period:

o If more than 30 days have elapsed since the previous “Align IF Cable” or “Align RRH Amplitude” alignments

o If the PXIe subsystem internal temperature has changed more than 5°C from the previous “Align IF Cable” or “Align RRH Amplitude” alignments

o If IF cables have been disconnected, reconnected, moved or replaced

 

Characteristics

 

Notes

 

• The characteristics provided in this data sheet for operation at or below 8 or 12 GHz are a subset of the specifications for the Keysight M9415A PXIe VXT Vector Transceiver module. For the most recent detailed performance information, refer to the M9415A Data Sheet (literature no. 3120-1518.EN). Note that the performance characteristics in that data sheet apply at the input/output connectors of the M9415A module, but in the S9130A system, there is approximately 0.25 to 0.5 dB of insertion loss between the S9130A front panel connectors and the M9415A due to the M9155C switch module and cabling.

• The M9415A-001 in this S9130A 5G Multi-Band Vector Transceiver is configured with:

o Option F08 (frequency range, 380 MHz to 8 GHz), or Option F12 (frequency range, 380 MHz to 12 GHz)

o Option B12 (1.2 GHz bandwidth)

o Option M05 (512 MSa memory)

o Option 1EA (High output power)

 

Definitions

 

Typical (typ)

Describes additional product performance information that is not covered by the product warranty. It is performance beyond specifications that 95% of the units exhibit with a 95% confidence level at room temperature (approximately 25 °C). Typical performance does not include measurement uncertainty. Typical performance is not warranted.

Nominal (nom)

Describes the expected mean or average performance, or an attribute whose performance is by design, such as the 50 Ω connector. This data is measured at room temperature (approximately 25 °C). Nominal performance is not warranted.

Measured (meas)

Describes an attribute measured during the design phase for purposes of communicating expected performance, such as amplitude drift vs. time. This data is measured at room temperature (approximately 25 °C). Measured performance is not warranted.