BreakingPoint Applications and Security Testing

데이터 시트

Problem: Real-Time Challenges for Real-World Testing

 

These days, organizations rely on a wide variety of security solutions to protect their networks from cyber-attacks and traffic anomalies. But the more tools deployed, the more complex a security infrastructure becomes. The result: a hodgepodge of security solutions that are tough to verify and challenging to scale. Worse yet, these complex system interactions pose a serious risk to security performance and network resiliency.

 

Solution: An Easy-to-Use Testing Ecosystem for Modern Network Needs

 

To counter such challenges, businesses require an application and security test solution that can verify the stability, accuracy, and quality of networks and network devices.

Enter BreakingPoint. By simulating real-world legitimate traffic, distributed denial of service (DDoS), exploits, malware, and fuzzing, BreakingPoint validates an organization’s security infrastructure, reduces the risk of network degradation by almost 80 percent, and increases attack readiness by nearly 70 percent.

How might a particular configuration or security setup withstand a cyber-attack? BreakingPoint addresses that by simulating both good and bad traffic to validate and optimize networks under the most realistic conditions. Security infrastructures can also be verified at high scale, ensuring ease of use, greater agility, and speedy network testing.

 

Highlights

 

  • Measure and harden the performance of network and security devices
  • Validate network and data center performance by recreating busy hour Internet traffic at scale
  • Stress network infrastructures with more than 190,000 security attacks, malware, botnets, and evasion techniques
  • Find network issues and prepare for the unexpected with the industry’s fastest protocol fuzzing capabilities
  • Emulate sophisticated, large-scale DDoS and botnet attacks to expose hidden weaknesses
  • Ensure the always-on user experience amid complexity and exploding traffic volume
  • Train staff by simulating highly realistic cyber-range/training environment
  • Validate the performance and security resiliency of service provider networks using emulations over 3G/4G/LTE 
  • Amplify test traffic realism by running TrafficREWIND summary configurations that replicate the dynamic nature of production networks and applications 

 

Key Features

 

  • Simulates more than 780 real-world application protocols
  • Allows for customization and manipulation of any protocol, including raw data
  • Generates a mix of protocols at high speed with realistic protocol weight
  • Offers HTTP1.0, HTTP1.1 and HTTP/2 as transport with support for NAT and Proxy (for selected applications)
  • Supports more than 190,000 attacks and malwares
  • Delivers from a single port all types of traffic simultaneously, including legitimate traffic, DDoS, and malware
  • Bi-monthly Application and Threat Intelligence (ATI) subscription updates ensure you are current with the latest applications and threats
  • Combined with the APS 100/400GE Series platform, BreakingPoint reaches a staggering performance with a fully-populated system — 3.2 Tbps / 5.1 billion sessions and 56 million connections per second — to emulate enterprise-wide networks to continent-scale mobile carrier networks
  • Leverage the hyperscale performance of the new APS-100/400GE Series platform. A single APS-ONE-100 delivers unparalleled real-world TLS performance of up to 100K TLS connections per second and 3.2M TLS concurrent connections and 150Gbps encrypted throughput. The ground-breaking scale of a 10-appliance system generates 1M TLS CPS, 32M TLS concurrent connections, and 1.5 Tbps encrypted TLS throughput.