Exposing Hidden Security Threats and Network Attacks

백서

Over the years, information technology (IT) departments have been implementing solutions that answer two questions:

 

  • How do I make as many services available to stakeholders as possible?
  • How do I protect and secure everything?

 

While some IT departments approach these as a dual mandate, others treat them as competing goals with tradeoffs. Sometimes security takes priority and other times new services are so powerful or transformative they are deployed immediately and secured with best efforts.

 

Cloud, virtualization, and mobility have brought a wave of vendors offering point solutions with benefits such as scalability and efficiency. At the same time, the number of security vendors offering advanced types of protection have exploded. While new trends in IT have increased availability and access to services, it has also shattered the traditional network boundary — data and assets no longer sit in a single location behind a firewall. As a result, many enterprises have erred on the side of there is no such thing as too much security, especially with the increased frequency and sophistication of attacks. A recent study of network management practices found nearly one-third of respondents are using 11 or more active tools.