E21-ac5v1
CVSS:
8.8 CVSS:3.1/AV:N/AC:L/PR:L/UI:N/S:U/C:H/I:H/A:H
False Positive:
t
Variants:
4
Year:
2020
Description
This strike exploits a command injection vulnerability in OpenEMR. This vulnerability is due to insufficient sanitation for the user-supplied data in the backup.php. A remote authenticated attacker can exploit this vulnerability by sending crafted requests to the target server. Successful exploitation could result in arbitrary command execution in the security context as web server.
*NOTE: When running this strike in OneArm mode, the requests will not be sent to /openemr/someuri , instead will be sent to /someuri , since the openemr server docker used, is configured that way.