Flyers
Keysight Expert Support Service Using AR Glasses
Keysight Expert Support Service is a new optional support service contract offering AR glasses with step-by step instructions through real time live video, messaging and voice interaction to guide customers to resolve technical issues efficiently.
This new support model offer “What You See Is What I See” concept to customers that allow Keysight’s expert consultant to remotely guide customers with issue resolution immediately without the need to be on-site.
What are the challenge customers are facing now?
The majority of customers think their experienced engineers can solve most issues. Urgent issues can to be supported via mobile phone or Web conferencing but, many customers still prefer to have an expert on-site immediately rather than troubleshoot with remote support.
The gap that customers do understand is customers need to do more preparations when our expert has been required on site. Repairing is also very difficult when it requires full of both technician’s hands and holding a Mobil phone.
Keysight’s New Approach
The new approach provides customers with live support from a Keysight expert consultant, enabling the on-site engineer to do the repairing and preventing any miscommunications that may arise when using mobile phones and Web conferencing.
With this new support model, customers get access to Keysight service and support immediately without waiting for an expert consultant to arrive on-site to troubleshoot. The Keysight expert consultant can now help customers to solve problems faster and minimize system downtime.
How Does It Work?
A pair of Keysight Technologies On-Site Now! is provided for the duration of the support service. Whenever a technical issue occurs, the on-site engineer gives connection permission to the remote Keysight expert consultant, thus giving the expert consultant a real-time view of the on-site situation via the smart glasses and the RemoteEye application. The remote expert consultant can then guide the technician resolve the issue with real-time visual, voice, and messaging, assistance. (At the end of the support service, simply return the smart glasses to Keysight.)
How to Manage Calls?
A support call normally starts over the phone and may progress through an online meeting or Web conferencing. At any time, you can ask to connect with the on-site engineer using the smart glasses. This is simply done by making a video call from your expert account home page which contains the list of your contacts (“on-site engineers” smart glasses). When needed, you can also invite guest experts to participate in the video call to troubleshoot the problem.
Security Protocols
Keysight Technologies On-Site Now! is protected by a suite of reliable and secure protocols — such as Secure Real-Time Transport Protocol (SRTP), Diagram Transport Layer Security–Secure Real-time Transport (DTLS-SRTP), 128-bit Advanced Encryption Standard (AES) to encrypt audio and video, HMAC-SHA1 to verify data integrity, Safe Harbor certified, and WebRTC technology.
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.