AI test case generation is the use of artificial intelligence to automatically create executable software tests from a model or specification of the system under test, rather than writing each test by hand. Modern implementations combine AI exploration with model-based testing: the AI traverses a digital twin of the application to identify paths, edge cases, and validation points, then generates ready-to-run tests.
This approach delivers broader coverage than manual test design and avoids the maintenance burden of script-heavy automation tools. Automation Intelligence (Eggplant Test) builds this model of the application and uses AI to generate and execute tests across the full state space.
Eggplant Test pairs AI exploration with a model-based testing engine. The model is the source of truth; the AI is what makes it productive.
Eggplant Test creates a digital twin of your app's screens, workflows, and decision points. This becomes the structural map the AI works against.
The AI engine traverses the model, identifying paths a human tester would miss and prioritizing scenarios by risk and coverage value.
Tests are produced from the model in formats ready to run in your existing pipeline. No manual script writing, no LLM hallucinations.
When the model updates, test cases regenerate. There's no script rewrite cycle, because there are no scripts to rewrite.
AI test case generation and AI test automation solve different problems. Test case generation is the design phase: AI analyses a model of the application to produce the executable tests themselves; defining what to test, in what order, and against which conditions. AI test automation is the execution phase: AI runs those tests, interacts with the application, and adapts to UI changes at runtime. Most modern testing platforms combine both, but the distinction matters when evaluating tools. Some excel at generation, others at execution, and the strongest deliver an integrated approach across both.
AI generates test cases by analyzing a model of the application (its screens, workflows, decision points, and possible user paths) and intelligently exploring that model to identify scenarios worth testing. Rather than replaying recorded actions or relying on a tester to enumerate every possibility, the AI prioritizes high-value paths, surfaces edge cases, and produces executable tests. The most reliable approaches use model-based testing as the foundation, which means generated tests remain deterministic and maintainable rather than relying on probabilistic LLM output that can hallucinate steps.
For most organizations, AI augments rather than replaces manual test case writing. AI excels at exhaustive path coverage, regression test generation, and identifying scenarios humans miss. Human testers remain essential for business-context validation and judgement calls on what to prioritize. The biggest productivity gains come from offloading repetitive test design to AI while keeping human attention focused on risk-based testing and nuanced verification. In practice, teams using AI test case generation typically expand their coverage rather than reduce headcount.
Model-based testing (MBT) is the engine behind reliable AI test case generation. MBT represents an application as a structured model of its behavior, states, transitions, inputs, and outputs. AI uses this model as the source of truth, exploring it to generate test cases that are deterministic, traceable, and maintainable. Without an underlying model, AI test generation tends to rely on LLM script synthesis, which can produce flaky tests and hallucinated steps. The combination of MBT and AI is what makes generated tests trustworthy at scale.
Accuracy depends entirely on the underlying approach. AI test case generation built on model-based testing produces deterministic, repeatable tests because the model itself defines what constitutes valid system behavior. AI generation that relies purely on large language models to synthesize test scripts is less reliable. These tools can produce tests that reference UI elements that don't exist or steps that won't execute. For production-grade automation, the MBT-plus-AI approach delivers the highest accuracy and the lowest maintenance burden over time.
AI test case generation delivers the strongest returns on complex, frequently changing applications where manual test design can't keep up with development velocity. Enterprise applications with deep workflows, regulated systems requiring high coverage (finance, healthcare, telecoms), cross-platform applications spanning multiple operating systems and devices, and modernization projects where legacy applications need test coverage retrofitted are all strong fits. Simpler applications with stable interfaces and small test surfaces may see less benefit; the productivity advantage scales with application complexity.
Können wir Ihnen behilflich sein?