Webinars
Learn the latest techniques for end-to-end power integrity digital twin simulations that are being driven by the technological growth in data centers, AI, and custom ASICs. Extreme dynamic currents when delivering 1000’s of Amps on sub 1-volt power rails can easily result in ground bounce and EMI crosstalk to victim nets. See how a digital twin Power Integrity EM model with a dynamic load can simulate both large signal and small signal behavior of a power delivery network to validate both power rail ripple and EMI crosstalk to adjacent victim nets.
Können wir Ihnen behilflich sein?