New i3070 Series 6 is 1.5x Faster than the Series 5

Applikationsberichte

Manufacturers are always looking to optimize their processes to reduce the cost of manufacturing their products. Time to market is a critical success factor as every second saved in test time is multiplied by the high volume, frequently thousands of units of products produced, deeply impacting manufacturing. Especially at these high volumes, machines used in manufacturing need to operate stably and reliably at high throughput. The Keysight i3070 Series 6 ICT is the test solution that meets manufacturing demands, improving test efficiency built upon the latest Control XTPB card, software supporting PathWave Manufacturing Analytics, Industry 4.0 Connected Factory Exchange IPC-CFX 2591, and machine-to-machine connectivity IPC-Hermes 9852.