How to Validate O-RAN Radio Unit Synchronization

Time Sync Analyzer
+ Time Sync Analyzer

O-RU Synchronization Plane Conformance

An Open Radio Access Network (O-RAN) radio unit synchronization-plane conformance test uses a configured synchronization source, an Ethernet fronthaul connection, and a controlled test environment. The radio unit under test exchanges timing information with the test platform while the engineer configures the Precision Time Protocol (PTP) profile, transport conditions, clock reference, and applicable synchronization parameters. A baseline acquisition sequence establishes the observed clock state. Test traffic and timing-related messages are captured for comparison with the selected O-RAN synchronization-plane test requirements. A shared reference, such as a pulse-per-second signal or a stable frequency input, provides a consistent timing basis during measurement.

The measurement sequence then exercises the device under defined operating and fault conditions. The engineer records synchronization state transitions, protocol responses, time-error behavior, and any relevant clock-quality metrics using the available timing interfaces. The test can include planned changes to clock-class information, source availability, or the received timing condition when supported by the installed software options. Results are evaluated against the specific conformance case and configuration rather than against a generic acceptance threshold. Packet observations and clock measurements must be correlated to distinguish message-processing failures from physical timing deviations. Repeatable setup parameters and stored results support comparison across hardware builds and firmware revisions.

O-RAN Radio Unit Synchronization Test Solution

O-RAN synchronization-plane conformance testing requires a controlled timing reference, an Ethernet interface to the radio unit, and a repeatable synchronization test sequence. The Keysight Time Sync Analyzer platform combines a rack-mount appliance, timing card, and Ethernet line card for test access. The O-RAN data sheet identifies the Time Sync Analyzer as part of a broader Open RAN Studio test environment. For dedicated synchronization-plane conformance, the installed option set must be checked to confirm that the required test functions are licensed. A test operator configures the timing source and port settings, runs a defined case, and examines timing states and captured protocol information. Depending on the configuration, an additional protocol generator or clock measurement option may be required. The arrangement supports structured validation of O-RAN radio-unit synchronization rather than relying on the base appliance alone.

Block Diagram of O-RAN Radio Unit Synchronization Test Solution

How to Validate O-RAN Radio Unit Synchronization - Block Diagram

Explore Products in Our O-RAN Radio Unit Synchronization Test Solution

Discover Resources and Insights

Additional Resources for O-RAN Radio Unit Synchronization Test

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?