How to Select DC-Coupled or DC-Blocked Power Sensors for RF Measurements

Average Power Sensors
+ Average Power Sensors

Select the Appropriate Sensor Coupling

Selecting the appropriate power sensor requires understanding whether direct current (DC) is present together with the radio frequency (RF) signal at the measurement point. A DC-coupled sensor presents a direct electrical path at its input, while a DC-blocked sensor incorporates a blocking capacitor that prevents DC from reaching the sensing circuitry. Using an unsuitable sensor configuration can affect measurement performance and, when DC is present at the measurement point, may expose a DC-coupled sensor to conditions that can damage sensitive components. Engineers should therefore evaluate both the RF signal and any DC component before connecting the sensor.

The measurement setup typically includes an average power sensor connected to a compatible power meter and the RF source or device under test. Engineers determine whether DC voltage may be present on the RF path, review the sensor input configuration and operating limits, and select the appropriate coupling architecture before making the connection. Matching the sensor configuration to the electrical characteristics of the test point helps engineers obtain reliable average power measurements while reducing the risk of measurement errors or sensor damage.

Average RF Power Sensor Selection Solution

Choosing between DC-coupled and DC-blocked sensing begins with evaluating the electrical conditions at the intended RF measurement point. Engineers identify whether the signal path carries RF only or combines RF with a DC component, then select a sensor architecture compatible with those conditions. A DC-blocked input prevents DC from reaching the sensor's measurement circuitry, while a DC-coupled configuration provides a direct input path and must be used within its specified electrical limits. The selected average power sensor is connected to a compatible power meter for measurement configuration, zeroing, calibration, and result display. Establishing the appropriate sensor configuration before connecting to the device under test provides a repeatable workflow for matching the measurement hardware to the signal path. This approach helps protect the measurement sensor, avoids inappropriate connections, and supports reliable average RF power measurements during component characterization, design verification, troubleshooting, and functional testing.

See Block Diagram of Average RF Power Sensor Selection Solution

Block Diagram - How to Select DC-Coupled or DC-Blocked Power Sensors for RF Measurements

Explore Products for Our Average RF Power Measurement Solution

Discover Resources and Insights

Additional Resources for Average RF Power Measurements

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?