How to Find Worst-Case Island Clearing Time

Regenerative AC / Grid Emulator
+ Regenerative AC / Grid Emulator

Locate Worst-Case Clearing Time

A worst-case clearing time search starts from a validated resonant island operating point with real and reactive power closely balanced. After measuring the baseline anti-islanding test result, the reactive component of the emulated load is adjusted incrementally to move the island resonance to either side of line frequency. A controlled reactive impedance sweep evaluates conditions below and above the baseline value in small steps. At every point, the inverter is returned to the required pre-island operating state, residual grid current is checked, the grid connection is opened, and the elapsed time to shutdown is measured. This produces a repeatable data set showing how anti-islanding response changes as the resonant-load condition moves away from its initial tuning. The same acquisition and shutdown criteria are maintained at every step so changes in the measured result can be attributed to the programmed impedance offset.

The sweep continues until the measured clearing-time trend decreases on both sides of the maximum region. The test system can then identify the longest-duration points and repeat them to verify the result and investigate possible non-detection zone behavior. Automated sequencing helps maintain the same setup, operating-point verification, island transition, waveform acquisition, and timing calculation for every test point. For IEEE 1547.1 evaluation, the resulting curve shows clearing-time sensitivity to reactive-load changes instead of representing the inverter with only one nominal load condition. Maintaining consistent tuning and measurement throughout the sweep also reduces the influence of operator-dependent adjustments when comparing results across a large number of repeated island events. Trend plots, captured waveforms, and repeated maximum points can then be reviewed together to confirm that the longest measured clearing time is reproducible.

Worst-Case Clearing Time Test Solution

The test requires a repeatable baseline island, programmable reactive-load offsets, and synchronized measurement at every point in the sweep. A regenerative grid-emulation platform can perform the reactive impedance sweep through programmable RLC behavior instead of requiring manual changes to physical inductors or capacitors. Test automation restores the specified pre-island condition, verifies residual grid current, initiates the island, records the shutdown waveform, and calculates worst-case clearing time for each operating point. Trend analysis can then identify the maximum region and the measurements that require additional repetitions. This workflow supports investigation of possible non-detection zone behavior while preserving comparable starting conditions across the sweep. For an IEEE 1547.1 anti-islanding test, coordinated emulation and measurement reduce repeated manual setup and provide a consistent method for evaluating how reactive-load changes affect clearing-time performance. Automated result storage also preserves the impedance offset, waveform record, and timing value for each repeated point in the maximum-clearing-time region.

See Block Diagram of Worst-Case Clearing Time Test Solution

How to Find Worst-Case Island Clearing Time

Explore Products in Our Worst-Case Clearing Time Test Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?