Automated IEEE 1547.1 Test

Data Sheets

As power demand increases, small, spread-out power generators called Distributed Energy Resources (DERs) continue to come online. For these DERs to provide power to the energy grid, they must comply to the many different regional standards. One such standard is IEEE 1547.1-2020 / UL 1741 SB which covers many different tests where compliance is required to connect into the electric utility (grid).

 

This is not a new test requirement. Solar and wind DERs, or any entity sending power to the grid, have been required to test to these standards for many years. They understand that testing to these standards is complex and time consuming. Newcomers to the DER market, such as V2G-enabled Electric Vehicles (EVs) and Electric Vehicle Supply Equipment (EVSEs), more colloquially known as charging stations, may not be familiar with the complexities.

 

This brochure aims to help both the seasoned grid compliance test engineers, as well as engineers that are performing these tests for the first time.

 

This brochure focuses specifically on the challenges of testing to IEEE 1547.1-2020 / UL 1741 SB and how Keysight can help you overcome these challenges in a new, innovative way that saves time, equipment, space, and money when compared to using traditional test equipment and methods.