How to Coordinate Multiple USB Power Sensors for Parallel RF Testing

USB Power Sensors
+ USB Power Sensors

Coordinate Multiple Power Measurements

Parallel radio frequency (RF) testing often requires power measurements at multiple test points or across several devices without moving a single sensor between measurement paths. Multiple USB power sensors allow each sensor to remain connected to its assigned RF measurement point while a common computer or test-system controller manages configuration and acquisition. This architecture eliminates the need for a separate hardware power meter for each sensor and reduces reconnection of RF interfaces during high-volume or multi-device testing. Engineers can incorporate multiple independent power measurements into an automated test sequence while maintaining a direct path between each signal and its associated sensor.

The measurement configuration includes multiple USB power sensors connected to separate radio frequency test points and a host computer used to communicate with the sensors. Engineers identify each connected sensor, establish the required measurement settings, perform zeroing as required, and coordinate acquisition through the test application. Measurement results from the individual sensors can then be collected and associated with the corresponding test point or device under test. This approach supports multi-device validation, production test, and automated systems where several radio frequency power measurements must be managed efficiently from a common controller.

Parallel RF Power Measurement Solution

A common host computer can manage multiple USB power sensors as individual programmable measurement resources within an automated radio frequency test system. Each sensor connects directly to its assigned measurement point and communicates digitally with the host, allowing the test application to configure sensors, initiate acquisitions, retrieve readings, and organize results without deploying separate hardware power meters. Standard Commands for Programmable Instruments can be used to address the connected sensors and incorporate their measurements into programmed test sequences, while measurement settings and averaging can be optimized according to the required speed and measurement conditions. Results can be collected by the host application for limit checking, comparison, storage, or reporting. This distributed sensor architecture reduces radio frequency reconnections and allows the test controller to coordinate measurements from multiple test points within the same workflow. It is suited to manufacturing and automated validation environments where increasing the number of power measurement points without multiplying conventional meter hardware can simplify system architecture and improve test efficiency.

See Block Diagram of Parallel RF Power Measurement Solution

See Block Diagram of Parallel RF Power Measurement Solution

Explore Products for Our Parallel RF Power Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?