Choose a country or area to see content specific to your location
애플리케이션 노트
Today’s integrated circuits (ICs) are designed with increasingly smaller geometries and higher processing speeds. These design features cause semiconductors to become increasingly vulnerable to electrostatic discharge (ESD) damage. ESD can be triggered by human touch, machine handling, testing by automated testers, or by pre-charge events such as friction produced by the handlers. ESD poses a serious threat to every IC design facility and fabrication process house. ESD-related failures are estimated to cost millions of dollars in lost revenue for IC manufacturers every year.
In battling ESD, factories are equipped with conductive flooring materials to conduct the electric charges from the work area. Operators handling ICs are required to wear special coats with conductive filaments, and/or heel-straps. At the work bench, operators are required to wear wrist straps to ensure that they are grounded. However, based on investigations by ESD experts, less than 0.10% of all the documented damage actually comes from ungrounded personnel touching ESD-sensitive products. In other words, 99.9% of ESD damage is attributed to charging/discharging events that occur in production equipment and processes. Consequently, maintaining ground integrity for equipment plays a vital role in the reduction of ESD.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.