How to Test Unintentional Island Clearing Time

Regenerative AC / Grid Emulator
+ Regenerative AC / Grid Emulator

Measure Island Clearing Time

An IEEE 1547.1 anti-islanding test begins by establishing a controlled operating point between a distributed energy resource (DER) inverter, grid emulator, and resonant load. Real and reactive power are balanced so residual grid current is minimized before the connection to the simulated utility is opened. The test system measures three-phase voltage, current, frequency, active power, reactive power, and phase behavior while maintaining the programmed grid condition. Accurate resistive, inductive, and capacitive behavior is required because island voltage and frequency depend on the interaction between inverter output and load impedance. These controlled conditions create repeatable unintentional islanding scenarios for DER inverter compliance testing while maintaining a defined electrical state immediately before grid isolation. The initial operating point also provides the reference needed to distinguish load-tuning effects from changes caused by the isolation event itself.

Once the operating point is stable, the grid connection is opened and the measurement system records the island clearing time from isolation to inverter shutdown. Voltage and current are monitored throughout the transition so the shutdown point can be identified from the measured waveforms. The procedure can then be repeated across specified operating conditions and load adjustments to characterize anti-islanding response. Automated grid emulator testing coordinates the grid condition, resonant load behavior, island transition, electrical measurements, and clearing-time calculation in a repeatable sequence. Maintaining consistent pre-island conditions at each test point makes it possible to compare shutdown behavior across multiple runs and determine how changes in island loading influence the measured clearing time. Captured waveforms and timing results can also be reviewed together to confirm that each reported clearing time corresponds to the same electrical definition of inverter shutdown.

Island Clearing Time Test Solution

The test requires a stable pre-island operating point, controlled grid isolation, and synchronized measurement of voltage, current, frequency, and shutdown timing. A regenerative AC / grid emulator provides the bidirectional three-phase power interface needed for grid emulator testing of connected DER equipment. Integrated Power Hardware-in-the-Loop functionality can reproduce the grid connection, switching event, measurement points, and resonant load behavior required for unintentional islanding without relying on a separate bank of manually adjustable passive components. Test automation coordinates the IEEE 1547.1 anti-islanding test, establishes repeatable initial conditions, initiates the island event, captures electrical measurements, and calculates island clearing time. The resulting workflow supports consistent DER inverter compliance measurements across repeated runs and varying island conditions while keeping grid emulation, load behavior, measurement acquisition, and analysis within a coordinated test environment. Result review can combine captured waveforms, measured electrical conditions, and calculated timing so repeated events can be compared with the same shutdown criteria.

See Block Diagram of Island Clearing Time Test Solution

Test Unintentional Island Clearing Time

Explore Products in Our Island Clearing Time Test Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?