How to Sequence Waveform Segments for Complex Stimulus

Expert Benchtop Waveform and Function Generator
+ Expert Benchtop Waveform and Function Generator

Build Repeatable Multi-Segment Stimulus Sequences

Complex device stimulus can contain repeated signal sections, changes in operating state, and event-dependent transitions that are difficult to manage as one continuous arbitrary waveform. The test definition must establish the individual waveform segments, their playback order, repeat behavior, and timing relationships so the overall waveform reproduces the intended sequence of electrical conditions presented to the device under test.

Long or conditional stimulus patterns also require predictable transitions between waveform sections without recreating the complete signal whenever the sequence changes. Individual segments may need to repeat continuously, play a defined number of times, or advance only after a specified event. Timing and waveform continuity must be maintained across segment boundaries so each test run presents the same complex stimulus to the device.

Complex Stimulus Waveform Sequencing Solution

Perform the test by dividing the required arbitrary waveform into reusable segments and defining the playback order, repeat count, and event conditions for each segment. An Expert Benchtop Waveform and Function Generator provides arbitrary waveform generation and waveform sequencing capabilities for constructing complex stimulus patterns from smaller waveform sections. Engineers can reuse and reorder stored waveform segments rather than recreating an entire waveform, repeat individual sections as required, and use trigger control to determine when the sequence advances to another segment. Waveform memory supports storage of the component segments, while sequencing reduces unnecessary duplication of repeated waveform data. The completed sequence provides repeatable playback of complex, multi-state stimulus patterns during device testing.

See Block Diagram of Complex Stimulus Waveform Sequencing Solution

Block Diagram of Complex Stimulus Waveform Sequencing Solution

Explore Products in Our Complex Stimulus Waveform Sequencing Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?