How to Measure Average Pulse Power with a Handheld Power Meter

Handheld RF Power Meter
+ Handheld RF Power Meter

Measure Average Pulse Power

Measuring average pulse power in a pulsed RF signal requires accounting for the relationship between average power and pulse timing. Unlike continuous-wave signals, pulsed signals alternate between active and inactive intervals, so power averaged over the full pulse repetition period differs from power during the active portion of the pulse. Engineers therefore need pulse width and pulse repetition period, or equivalent duty-cycle information, together with measured average power to calculate average pulse power. This approach is appropriate when pulse timing is known and the objective is average pulse power rather than peak power or detailed analysis of the pulse envelope.

The measurement setup can use a handheld RF power meter with an integrated sensor to acquire the average power of the pulsed signal. Engineers set the signal frequency, verify that applied power falls within the supported measurement range, and measure average power across repeated pulse cycles. The known pulse timing information is then combined with the measured average value to calculate average pulse power. This portable approach eliminates the need for a separate sensor and benchtop power meter, making it practical for field or space-constrained measurements while maintaining a clear distinction between average pulse power and instantaneous peak power.

Average Pulse Power Measurement Solution

Average pulse power measurements can be performed with a compact handheld instrument by combining average radio frequency power measurement with known pulse timing information. Engineers connect the pulsed signal directly to the integrated measurement input, configure the appropriate signal frequency, and acquire the average power reading across the pulse repetition interval. Pulse width and pulse repetition period are then used to account for the signal duty cycle and determine the corresponding average pulse power. The integrated sensor, local display, battery operation, and internal power reference support this workflow without requiring a separate external power sensor or benchtop meter. Engineers can perform self-calibration before measurement and view power readings directly at the test location, making the approach suitable for field verification, installation, maintenance, and portable engineering measurements. The workflow is intended for average pulse power determination when pulse timing is known; detailed peak-power, pulse-shape, rise-time, or fall-time characterization requires measurement capabilities beyond this average-power method.

See Block Diagram of Average Pulse Power Measurement Solution

How to Measure Average Pulse Power with a Handheld Power Meter Block Diagram

Explore Products in Our Average Pulse Power Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?