Official Used
Equipment Store

Resource Guide

What is a Capacitor? Uses & Functions Explained

Table of contents
更新于: 12月 08, 2025
Callum Reed
Used Equipment Store Marketing Manager
欢迎反馈
Stay Up to Date on Used Equipment!

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Get Email Updates
Second-Hand. First-Class.

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Why Buy From Keysight

Introduction

Choosing the right capacitor for your design and identifying whether a failing component is causing circuit instability are challenges every engineer faces.

Whether you're refining a power supply, filtering out noise, or optimizing signal timing, understanding capacitors at a deeper level is essential for making smarter engineering decisions.

This guide goes beyond textbook definitions to offer clear, actionable insights into how capacitors really function in electronic circuits. 

We will cover how they store and release energy, block DC while passing AC, and support everything from voltage smoothing to signal coupling. You will learn how different capacitor types behave under stress, how to troubleshoot common failure symptoms, and what specifications truly matter when you're choosing parts.

Whether you're an engineer trying to boost system reliability, a student building your foundation, or a procurement specialist sourcing the right component, this guide will give you the confidence to evaluate, apply, and maintain capacitors more effectively.

Understanding Capacitor Fundamentals

A capacitor is a passive electronic component that stores and releases electrical energy. It plays a foundational role in almost every circuit you’ll design, build, or troubleshoot. From smoothing voltage in power supplies to isolating AC signals in amplifiers, capacitors help manage power, stabilize signals, and improve performance.

At the core, a capacitor consists of two conductive plates separated by an insulating material called a dielectric. When voltage is applied across the plates, electric charge accumulates, creating an electric field and storing energy.

To use capacitors effectively, it’s important to understand their key specifications:

  • Capacitance: Measured in picofarads (pF), nanofarads (nF), or microfarads (µF), this defines how much charge the capacitor can store.
  • Voltage rating: The maximum voltage the capacitor can withstand without breakdown.
  • Polarity: Some capacitors (e.g., electrolytic and tantalum) are polarized and must be installed in the correct direction.
  • Equivalent Series Resistance (ESR): Represents internal resistance, affecting capacitor behavior at high frequencies.
  • Leakage current: The small amount of current that flows through the dielectric even when the capacitor is charged.

You will often see capacitors marked with coded values and polarity indicators. On schematics, they are typically represented by two parallel lines (non-polarized) or one straight and one curved line (polarized).

For a deeper understanding of how capacitance is calculated and how different variables affect it, visit the Keysight Knowledge Base on Capacitance Formulas.

Different Types of Capacitors and Their Construction

Capacitors come in various forms, each suited to different applications. The construction and dielectric material directly affect reliability, frequency response, and failure modes.

Common Capacitor Types

  • Ceramic capacitors: Use ceramic dielectric materials. Known for low ESR, stability, and wide frequency response. Common in decoupling and high-frequency applications.
  • Electrolytic capacitors: Offer high capacitance in a compact form. These are polarized and ideal for bulk energy storage but are sensitive to temperature and aging.
  • Film capacitors: Use plastic film dielectrics. They are non-polarized and excellent for applications requiring low distortion and high stability, such as audio circuits.
  • Tantalum capacitors: Compact and stable with relatively low ESR. However, they are more prone to catastrophic failure if overstressed.
  • Supercapacitors (ultracapacitors): Provide extremely high capacitance values and fast charge/discharge rates. Perfect for short-term energy storage and backup power.

Polarized vs. Non-Polarized Capacitors

  • Polarized capacitors (electrolytic, tantalum) must be installed with the correct polarity. Reversing polarity can cause leakage or failure.
  • Non-polarized capacitors (ceramic, film) can be used in either direction, making them suitable for AC signal paths.

Lifespan and Failure Modes

Each type has different longevity and failure behaviors:

  • Electrolytic: Prone to drying out and increased ESR over time.
  • Ceramic: Can crack due to mechanical stress; stable otherwise.
  • Film: Long lifespan, but large in size.
  • Tantalum: Sensitive to surge currents.
  • Supercapacitors: Limited by cycle life and voltage balance.

Quick Selection Tips

  • Use ceramic for high-frequency decoupling near ICs
  • Choose electrolytics for power supply filtering
  • Go with film capacitors for precision and audio paths
  • Opt for supercapacitors in energy buffering or backup storage

ENA Vector Network Analyzers

Perfect Signals, Perfect Performance

See E5080B Special Offers

How Capacitors Work in Practical Circuits

Capacitors aren’t just theoretical, they serve real, measurable purposes in your circuits:

Key Capacitor Functions

  • Energy storage: Absorbs brief bursts of energy when power fluctuates.
  • Filtering and smoothing: Reduces ripple in DC power supplies by averaging out voltage changes.
  • Signal coupling: Allows AC signals to pass between stages while blocking DC offsets.
  • Timing and frequency shaping: Used in RC and LC networks to create oscillators or time delays.

DC Blocking and AC Passing

When placed in series with a signal path, a capacitor blocks any DC voltage but allows AC signals to pass. This is critical in audio, RF, and mixed-signal designs.

Frequency Response and Noise Suppression

Capacitors influence frequency response in filters—low-pass, high-pass, band-pass. In digital circuits, bypass capacitors placed near power pins suppress high-frequency noise and maintain signal integrity.

Real-World Example: 0.1 µF Bypass Capacitor Near a Microcontroller

A 0.1 µF (100 nF) ceramic capacitor is commonly placed between the Vcc (power supply) and GND (ground) pins of a microcontroller. This configuration forms a bypass capacitor—sometimes referred to as a decoupling capacitor—and it plays a critical role in maintaining power integrity at the chip level.

When a microcontroller switches states (e.g., toggling digital outputs or processing internal logic), it creates sudden changes in current demand. These rapid transitions can introduce transient voltage fluctuations or high-frequency noise on the power supply rail, which may lead to erratic behavior or logic errors.

The 0.1 µF capacitor addresses this by providing a local reservoir of charge close to the microcontroller. Because it is physically close and has low equivalent series inductance (ESL), it can quickly supply or absorb current during transients. This response is much faster than a regulator or bulk capacitor located further away on the board.

Key characteristics that make the 0.1 µF ceramic capacitor ideal for this application:

  • Low ESR and ESL: Enables rapid response to high-frequency transients.
  • High-frequency effectiveness: 0.1 µF is well-suited to suppressing noise in the 10 MHz to 100 MHz range, common in digital switching.
  • Small size and low cost: Fits easily on PCBs, including directly beneath ICs with via-in-pad routing.

In most designs, it's recommended to place one 0.1 µF capacitor per power pin as close as possible to the IC, ideally within a few millimeters. This helps isolate each component from shared power supply noise and reduces the risk of ground bounce and voltage dips.

Multiple decoupling capacitors of different values (e.g., 0.01 µF, 0.1 µF, and 10 µF) are often used together to cover a broader frequency range, improving noise suppression across the board.

RF Signal Generators

Real-World Signal Testing

See N5172B Special Offers

Key Applications of Capacitors in Engineering Projects

Capacitors are essential components across nearly all areas of electrical and electronic engineering. Their unique ability to store and release energy, filter signals, and manage voltage transitions makes them indispensable in both analog and digital systems. 

Below are the most important real-world applications where capacitors are actively deployed:

Power Supplies and Voltage Stabilization

In regulated power supplies, capacitors are used for smoothing and filtering. After rectification, they help reduce ripple in the DC output by temporarily storing charge and releasing it during voltage dips. 

Bulk electrolytic capacitors are typically used for low-frequency smoothing, while ceramic capacitors near the output provide high-frequency filtering.

Motor Starters and HVAC Systems

Large capacitors, particularly start and run capacitors, are used in single-phase AC motors found in HVAC units, compressors, and pumps. 

These capacitors shift the phase of the voltage between motor windings, creating a rotating magnetic field to start or boost the motor. Oil-filled film capacitors are often chosen for their durability and high voltage tolerance in these applications.

Audio and Communication Systems

In analog audio and RF circuits, capacitors are crucial for signal coupling and DC blocking between amplifier stages. They also serve in filter circuits, allowing certain frequencies to pass while attenuating others. 

Film capacitors and Class 1 ceramics are preferred in audio for their low distortion and stability. In communication systems, multilayer ceramic capacitors (MLCCs) are widely used for decoupling and noise suppression.

Supercapacitors for Energy Storage

Supercapacitors (ultracapacitors) are used where rapid charge/discharge cycles are required, such as in energy harvesting, memory backup, regenerative braking systems, or short-term uninterruptible power supplies. 

Their high power density and long cycle life make them ideal for bridging power interruptions or smoothing output in renewable energy systems.

For deeper technical examples in power electronics, see Keysight’s application note on high-efficiency power designs.

Capacitor Types vs. Common Industry Applications

Capacitor Type Key Applications Typical Characteristics
Ceramic Decoupling, high-frequency filtering, RF modules Small, low ESR, stable at high frequencies
Electrolytic Power supply filtering, bulk energy storage High capacitance, polarized, larger size
Film Audio signal paths, motor run/start, power factor correction Low distortion, long life, high stability
Tantalum Compact designs, timing, bypass in portable electronics Stable, low ESR, polarized, voltage-sensitive
Supercapacitor Short-term energy storage, memory backup, regenerative loads High capacity, rapid cycling, large form

Selecting the Right Capacitor for Your Project

Choosing the right capacitor is more than matching values on a schematic. Each application has performance, reliability, and environmental demands that affect capacitor selection.

Critical Selection Factors

  • Voltage rating: Always choose a rating at least 20–50% higher than the expected operating voltage.
  • Capacitance: Choose based on the required charge or timing characteristics of the circuit.
  • Tolerance: Indicates how much the actual capacitance can vary from the stated value. ±10% is common, but tighter specs are available.
  • Equivalent Series Resistance (ESR): Lower ESR is better for high-frequency or high-current applications.
  • Temperature range: Ensure the capacitor operates reliably across your system's environmental conditions.

Reading Capacitor Datasheets

When reviewing datasheets, look for:

  • Rated capacitance and voltage
  • Operating temperature range
  • ESR at specific frequencies
  • Leakage current
  • Endurance/lifetime ratings (e.g., hours at 105°C)
  • Dielectric material and construction details

Common Pitfalls to Avoid

  • Ignoring temperature derating, which can reduce capacitance or shorten life.
  • Overlooking ESR, especially in switching regulators or high-frequency circuits.
  • Assuming larger capacitance is always better, which can introduce unwanted slow response or startup issues.

Step-by-Step Selection Checklist

  1. Define your circuit’s required voltage, frequency, and current characteristics
  2. Determine ideal capacitance value and tolerance range
  3. Identify operating temperature range and potential thermal stress
  4. Choose dielectric type based on stability and application
  5. Confirm size, mounting type (through-hole or SMD), and packaging
  6. Evaluate ESR and leakage current based on signal sensitivity
  7. Review supplier datasheets and reliability metrics

Evaluating Suppliers for Capacitors

  • Choose vendors with full traceability and certified test data.
  • Ensure availability of long-term production or alternatives.
  • Look for responsive technical support and failure analysis capabilities.
  • Prioritize suppliers that offer quality assurance and compliance with relevant standards (e.g., RoHS, AEC-Q200 for automotive).

For an interactive and visual breakdown of capacitor behavior and selection principles, refer to this helpful MIT capacitor guide.

Troubleshooting and Maintenance of Capacitors

Capacitors, while generally reliable, are still prone to degradation and failure over time, especially in high-temperature or high-voltage environments. Knowing how to spot failure symptoms and test suspect components helps you prevent circuit faults, improve uptime, and extend equipment life.

Common Symptoms of Failing Capacitors

Watch for these signs during visual inspection or circuit diagnostics:

  • Bulging or swollen casing: Often seen in electrolytic capacitors, this indicates internal gas buildup due to overheating or aging.
  • Leaking electrolyte: Corrosive fluid may seep from the base or vent, damaging nearby PCB traces.
  • Burn marks or discoloration: Evidence of overheating, often related to current surges or excessive ESR.
  • Circuit instability: Symptoms include erratic behavior, power loss, unexpected resets, or output ripple in power supplies.
  • Open or short circuit behavior: May cause total failure of a signal path or power rail.

Hands-On Testing Methods

  1. Visual inspection: Start with the simplest method—look for deformation, corrosion, or damage.
  2. ESR meter testing: Measures the capacitor’s equivalent series resistance. A high ESR value often indicates a failing capacitor, even if capacitance appears correct.
  3. Capacitance measurement: Use a digital multimeter with capacitance mode or an LCR meter to verify actual capacitance. For a detailed walkthrough, see our guide on how to test a capacitor.
  4. In-circuit testing: Some ESR meters and testers allow for capacitor analysis without desoldering, though readings may be affected by surrounding components.

Preventative Maintenance Best Practices

Maintenance strategies vary by capacitor type and application:

  • Electrolytic capacitors: Replace every 5–10 years in high-temperature environments or as specified in datasheets. Store in sealed packaging until installation.
  • Film and ceramic capacitors: Inspect for mechanical stress or board flexing that may cause microcracks.
  • Supercapacitors: Monitor for voltage balancing and discharge rate consistency. Use balancing circuits in series configurations.

Keep detailed service logs and track in-field failure rates. In critical systems, replace aging capacitors during scheduled downtime rather than waiting for signs of failure.

When to Escalate or Upgrade

Escalate to the manufacturer when:

  • Repeated failures occur in a specific model or batch
  • Failures occur before rated endurance
  • Performance degradation affects system safety or compliance

Consider upgrades if:

  • The capacitor’s voltage rating is marginal for the application
  • ESR or leakage current is causing efficiency losses
  • Better dielectrics or ruggedized designs are available for your environment

Advanced Considerations for Professional Engineers

For engineers working in high-reliability, high-frequency, or long-lifecycle applications, surface-level capacitor knowledge isn’t enough. 

Understanding second-order effects and modeling capacitor behavior under real-world conditions is essential for ensuring robust, efficient, and predictable system performance.

Dielectric Absorption, Leakage, and Aging

In demanding applications, long-term stability can be just as important as initial performance. Several capacitor characteristics can degrade over time or affect precision circuit behavior:

  • Dielectric absorption is the tendency of a capacitor to retain a small residual charge after being discharged. This can introduce voltage errors in precision analog circuits and timing errors in sample-and-hold applications.
  • Leakage current refers to the steady-state current that flows through the dielectric. Over time, this can drain charge and alter timing or energy storage. Tantalum and electrolytic capacitors generally have higher leakage than ceramic or film types.
  • Aging effects are most significant in Class II and III ceramic capacitors (such as X7R or Y5V), which exhibit gradual, logarithmic capacitance loss. This process is accelerated by heat and mechanical stress. For applications requiring long-term stability, film capacitors or Class I ceramics are better suited.

High-Frequency Performance and Thermal Management

At high frequencies, parasitics such as equivalent series inductance (ESL) become dominant. Capacitor impedance increases with frequency due to ESL, making component selection and placement critical in RF and fast-switching power designs.

To optimize performance:

  • Use multilayer ceramic capacitors (MLCCs) with low ESL for decoupling.
  • Combine capacitors of different values (e.g., 0.01 µF, 0.1 µF, 10 µF) to cover a wider frequency spectrum.
  • Place capacitors close to high-speed switching nodes and minimize trace inductance.
  • Monitor surface temperatures; excess heat shortens life, especially in electrolytics.

In high-power circuits, consider thermal derating and apply heat-sinking or airflow strategies for temperature-sensitive capacitor types.

Simulation Techniques

Capacitor behavior can be modeled in SPICE or equivalent tools using RLC equivalent circuits that account for ESR, ESL, and leakage. Advanced models also include temperature and frequency dependencies, especially for ceramics and polymer hybrids.

Using accurate simulation helps:

  • Predict resonance points
  • Evaluate transient response
  • Assess performance under ripple current stress
  • Optimize decoupling networks before physical prototyping

Innovations in Supercapacitor Design

New developments in graphene-based supercapacitors, solid-state electrolytes, and hybrid lithium-ion capacitors are extending energy density, safety, and cycle life. These technologies offer exciting possibilities for backup power, energy harvesting, and portable electronics.

For a deep dive into current research, see this IEEE article on recent capacitor innovations.

Conclusion

Capacitors are critical to the performance, stability, and efficiency of nearly every electronic system. Whether you’re managing voltage in a power supply or filtering signals in communication hardware, understanding how capacitors work (and how to choose the right one) can make or break your project.

In this guide, we covered the fundamentals of capacitor construction and behavior, explored real-world applications, and provided advanced insights on aging, ESR, and high-frequency performance. We also outlined practical strategies for selecting, testing, and maintaining capacitors across a wide range of environments and circuit demands.

For engineers who want to design with confidence, sourcing high-quality components is just as important as technical know-how. That’s where Keysight can help. 

Visit the Keysight Used Equipment Store to browse certified pre-owned oscilloscopes, LCR meters, and signal analyzers—refurbished to OEM standards and backed by industry-leading warranty and support.

Make smarter component decisions. Test with precision. Build with confidence.

Whenever You’re Ready, Here Are
5 Ways We Can Help You

2

Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri

3

Contact our sales support team

4

Create an account to get price alerts and access to exclusive waitlists

5

Talk to your account manager about your specific needs.

Frequently Asked Questions

Dielectric materials determine a capacitor’s stability, size, temperature behavior, and long-term reliability. For example:

  • Class I ceramics (C0G/NP0) are stable and low loss, ideal for precision circuits.
  • Class II ceramics (X7R, Y5V) offer higher capacitance but can vary with temperature and voltage.
  • Tantalum and electrolytic capacitors provide higher capacitance but are more sensitive to temperature and polarity.
  • Film capacitors are excellent for audio and power applications due to their low distortion and thermal stability.

ESR (Equivalent Series Resistance) varies widely:

  • Ceramics: Very low ESR (<0.01 Ω)
  • Tantalum: Moderate ESR (0.01–0.1 Ω)
  • Electrolytic: Higher ESR (0.1–1 Ω)

High ESR can cause excessive heat, reduced filtering efficiency, and instability in switching power supplies. For high-frequency or high-current designs, always select capacitors with low ESR.

Use supercapacitors when you need:

  • Rapid charge/discharge cycles
  • High power density (but not energy density)
  • Short-term backup power or energy buffering

They are ideal in applications like memory backup, regenerative braking, and energy harvesting, but unsuitable for AC coupling or precise timing.

Temperature affects:

  • Capacitance stability (especially in ceramics)
  • ESR increase at low temps
  • Accelerated aging at high temps

Always select capacitors with an appropriate temperature rating and derate where necessary. Excessive heat shortens lifespan, especially for electrolytics.

Common failure modes include:

  • Overvoltage or incorrect polarity
  • Excessive ripple current
  • Thermal stress or poor ventilation
  • Aging and electrolyte dry-out
  • Mechanical damage (e.g., board flex cracks in ceramics)

  • Use a resistor-rated discharge tool (typically 1–10 kΩ, 1–5 W)
  • Avoid shorting terminals with metal tools
  • Wait several seconds and verify with a voltmeter
  • For high-voltage systems, follow lockout/tagout procedures

  • Use ruggedized or automotive-grade capacitors (e.g., AEC-Q200 certified)
  • Apply thermal management strategies (heatsinks, airflow)
  • Select long-life or solid electrolytic types with high endurance ratings
  • Avoid mechanical stress during board assembly and handling

Yes. Look for:

  • RoHS and REACH compliance
  • AEC-Q200 for automotive
  • UL and CE marks for safety
  • IEC/EN 60384 for film capacitors
  • Manufacturer datasheets often specify qualification and compliance testing

  • Source from authorized distributors or OEMs
  • Verify markings, lot codes, and datasheets
  • Request certificate of conformance
  • Watch for abnormally low prices or inconsistent physical sizes
  • Consider incoming inspection and sample testing for large orders

Capacitors in power supplies:

  • Filter ripple after rectification
  • Stabilize voltage output under load
  • Reduce switching noise (ceramic MLCCs near regulators)
  • Prevent voltage dips during sudden load increases

Bulk capacitors (electrolytics or film) handle low-frequency variations, while ceramic bypass capacitors suppress high-frequency noise close to ICs.

Callum Reed
Used Equipment Store Marketing Manager
欢迎反馈
Stay Up to Date on Used Equipment!

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Get Email Updates