DSP Research Scales 5G RF Regulatory Certification with Automated Testing

Case Studies

DSP Research selected Keysight's 5G device test solutions to deliver RF regulatory certification services in Japan. The Keysight E7515B UXM 5G Wireless Test Platform, running the S8711A Test Application software, automates testing and validation of devices to MIC specifications for RF interference, saving DSP Research time.

 

Under Japanese law, mobile devices must be certified that they do not transmit RF power outside their allocated frequency band before they can be connected to telecommunications networks. DSP Research provides this certification for 5G devices such as smartphones, laptops, and wearables against specifications set by the Ministry of Internal Affairs and Communications (MIC), ensuring interference with other radio services is limited.

 

With rapidly evolving 5G specifications and an explosion in the number of connected devices, DSP Research faced growing challenges scaling its certification services to meet increased demand.

DSP Research needed a way to automate testing and validation against MIC specifications, expand its coverage of smartphone certifications, and keep pace with evolving 5G regulatory test methodologies.

 

Keysight helps DSP Research meet this challenge with the E7515B UXM 5G Wireless Test Platform running the S8711A Test Application software.

The Keysight E7515B UXM 5G Wireless Test Platform saves DSP Research time by automating testing and validation of devices to MIC specifications for RF interference.

 

DSP Research is also leveraging Keysight's global expertise in device testing and validation to increase coverage of smartphone certifications where vendors have been pre-validated, as well as to address evolving 5G regulatory test methodologies.