M9485A PXIe Multiport Vector Network Analyzer

Configuration Guides

M9485A PXIe Multiport

Vector Network Analyzer

Ordering Guide

The following steps will guide you through configuring your M9485A.

Step 1. Choose primary receiver type and its number of port (mandatory). If two or three of receiver type is required, use step 2 to add the receiver.

Step 2. Choose additional receiver (multiple test sets can be ordered if needed).

Step 3. Add an M9300A PXIe frequency reference

Step 4. Choose software option

Step 5. Add a chassis

Step 6. Add a PCIe cable interface for 2-chassis configuration

Step 7. Select controller (either embedded controller or via PC)

Software Upgrades

Hardware Upgrades

Refer to M9485A Post-Purchase Upgrades in Keysight.com for adding port configurations.

Literature Resources

Web Resource

Get the latest news, product and support information, application literature and more.

http://www.keysight.com/find/m9485a

http://www.keysight.com/find/pxivna