Discusses the latest innovations in PathWave Device Modeling (IC-CAP) software. Covers topics such as the redesigned user interface, the support for Python 3, and the integration with customized installations. Also discusses the use of IC-CAP to extract compact models for a variety of semiconductor devices, including CMOS, bipolar, and compound semiconductors.