As digital transformation accelerates, QA teams face the impossible task of testing faster, broader, and more intelligently — across multiple platforms, integrations, and continuous releases. Traditional automation helps but still relies heavily on manual scripting, maintenance, and interpretation. It cannot keep pace with constant UI changes, growing data volumes, and the speed of modern development. The result is a cycle of rework, missed coverage, and delayed releases. What’s needed is not more automation, but smarter automation.
Keysight Eggplant Test delivers precisely that through AI-augmented testing – an approach that combines human expertise with artificial intelligence to design, execute, and optimize tests faster and more intelligently. Rather than replacing testers, Eggplant’s AI acts as a co-pilot, accelerating every stage of the testing lifecycle. It automates test creation from natural-language requirements, executes tests through human-like visual interaction, self-heals when software changes, and continuously learns from every run to improve accuracy and coverage.
At the heart of this approach are four key AI capabilities:
- Keysight Generator – Converts user stories and requirements directly into executable test cases using natural language understanding, drastically reducing test design time.
- Computer Vision and Fusion Engine – Interacts with software visually, just like a human user, validating real UI behavior across any device or environment.
- AI Self-Healing – Automatically adapts broken or outdated tests to evolving UIs and element changes, minimizing maintenance effort.
- AI-Driven Analytics – Detects unstable tests, coverage gaps, and risk patterns to continuously optimize testing efficiency.
- This AI-augmented process transforms testing into an adaptive, data-driven cycle. Eggplant ingests requirements, generates and executes tests automatically, and applies continuous feedback to refine coverage. Over time, it builds a self-optimizing testing ecosystem that accelerates release cycles while enhancing reliability and insight.
- The impact spans the entire organization. QA engineers gain freedom from repetitive scripting and maintenance, focusing instead on analysis and exploration. Testing managers gain stability, traceability, and targeted visibility into quality risks. Executives see measurable ROI through shorter release cycles, reduced costs, and higher customer satisfaction. By integrating seamlessly with CI/CD pipelines, Eggplant ensures every deployment is validated proactively — making continuous testing a reality.
- American Electric Power (AEP) offers a compelling example of AI-augmented testing at scale. Using Eggplant, AEP modernized QA across 55 applications, reducing test execution time by 75%, identifying 82 critical defects before production, and saving $1.2 million annually compared with Selenium-based testing. Even non-technical business users were able to generate and execute tests in minutes—extending automation beyond QA teams and directly improving business outcomes.
- With AI-augmented testing, Eggplant transforms QA from a manual checkpoint into an intelligent, self-learning process that evolves with your software. The result is continuous confidence — where every release is faster, every test is smarter, and quality becomes a competitive advantage.