Vision Edge 400P (Model: Vision E400P) NextGen Network Packet Broker

Data Sheets

Vision E400P supports advanced packet processing that includes advanced packet manipulation at line rate, such as header stripping (removing protocol encapsulations), deduplications (detecting and removing packet duplicates), packet trimming (only sending specified number of bytes for every packet), timestamping (replacing MAC source with timestamp), data masking (masking part of the packet), and tunneling (sending packets over L2GRE or VxLAN tunnels)