E19-7nvx1
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2019
Description
This strike exploits an SQL injection vulnerability in Zoho ManageEngine Applications Manager. The vulnerability is caused by insufficient validation of user input "resourcetype" on HTTP requests which are used to create SQL queries. Successful exploitation could allow an attacker abilities to execute SQL queries on the target server.