Choose a country or area to see content specific to your location
What are you looking for?
3D Interconnect Designer provides a flexible modeling and optimization environment for any advanced interconnect structure, including chiplets, stacked die, packages, and PCBs.
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
Explore the complete portfolio of Keysight software, from design engineering tools to emulator and instrument software, built to extend and enhance your Keysight instruments. Whether you are configuring measurements, automating tests, analyzing data, or validating compliance, use the filters below to identify the right software to support your workflow — from design and validation through manufacturing and deployment.
No Filter available
No Filter available
No Filter available
Eliminate design cycles by creating real-world power device models resulting in simulations you can trust.
Eliminate design cycles by creating real-world power device models resulting in simulations you can trust.
PD1000A
Eliminate design cycles by creating real-world power device models resulting in simulations you can trust.
The hybrid-electric and electric vehicle (HEV / EV) market is growing rapidly. Increasing vehicle electrification in the automotive market brings new challenges in design and manufacturing. Many HEV and EV manufacturers are migrating their power-conversion designs to wide bandgap (WBG) devices, such as silicon-carbide and gallium-nitride, to gain higher efficiency (extended range) and higher power in smaller, lighter, and cooler packages. However, there are significant concerns about making sure these new designs are reliable and safe.
Keysight is partnering with industry leaders in the HEV / EV power-conversion market to help them transition smoothly to using WBG devices in their designs. As a result of these relationships, Keysight has developed a state-of-the-art modeling suite of power circuit simulator tools that allow WBG device designers to easily create models never before possible. The test suite, which consists of curve-tracing, S-parameter, and double-pulse tester hardware, takes measurements from WBG devices and uses advanced software to build sophisticated simulation models that are exclusive to Keysight. These simulation models can be used in Keysight’s Advanced Design System software to simulate and analyze the effects that high-frequency components have on the reliability and electromagnetic interference of the design. Design changes can be made before the first prototype, saving time and cost by eliminating unnecessary design cycles.
Built for power converter design for power generation and transmission, aerospace-defense, automotive, data center, consumer electronics, and IoT applications.
Built for power converter design for power generation and transmission, aerospace-defense, automotive, data center, consumer electronics, and IoT applications.
W3035E
Built for power converter design for power generation and transmission, aerospace-defense, automotive, data center, consumer electronics, and IoT applications.
The W3035E PEPro includes:
Keysight’s solution for power electronics includes analysis capabilities such as electromagnetic solvers that enable the simulation of board effects from layout parasitics. New in the Power Electronics Pro (PEPro) design suite is an inner layer near-field visualization, very important to look at the currents and fields for long-term reliability. You can discover areas of current constriction, which may cause heating effects and affect reliability. The analysis of the boards supports both the method of moments (MoM) planar simulation, as well as a finite element method (FEM) for 3D effects.
Note: This element license requires a host bundle to work. For recommended bundle configurations, click here.
The W3631B is designed for power converter design for power generation and transmission, AD, automotive, data center, consumer electronics, and IoT applications.
The W3631B is designed for power converter design for power generation and transmission, AD, automotive, data center, consumer electronics, and IoT applications.
W3631B
The W3631B is designed for power converter design for power generation and transmission, AD, automotive, data center, consumer electronics, and IoT applications.
The W3631B ADS Core, EM Design, Layout, PEPro, PE Ckt Sim includes:
Keysight’s solution for power electronics includes both device modeling and power electronics simulation, and includes Power Electronics Pro (PEPro) analysis capabilities such as harmonic balance for precise analysis of periodic steady state signals and closed loop analysis. It also includes transient design simulation for analysis of the switching characteristics including the open loop analysis. The electromagnetic (EM) solver enables the simulation of board effects from layout parasitics. New in the PEPro design suite is an inner layer near-field visualization, very important to look at the currents and fields for long-term reliability. You can discover areas of current constriction, which may cause heating effects and affect reliability. The analysis of the boards supports both the method of moments (MoM) planar simulation, as well as a finite element method (FEM) for 3D effects.