Choose a country or area to see content specific to your location
애플리케이션 노트
In the early 2000s, ball grid array and accessible Surface Mount Technologies (SMT) components were the standard on most printed circuit board assemblies (PCBAs). At that time, Keysight’s Vectorless Test Enhanced Probe (VTEP) was a real breakthrough for increasing coverage for in-circuit test. But nowadays, the integrated circuits (ICs) and accessible surface mount device (SMD) components are getting smaller such that they could be mounted onto PCBAs. This causes the spaces to condense; and the fixture density increases which limit the sensor plate and amplifier placement.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
브라우저 쿠키가 만료되거나 브라우저 캐시가 지워지면 액세스 권한이 초기화됩니다. 콘텐츠에 다시 액세스 하시려면 다시 로그인하세요.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.