Choose a country or area to see content specific to your location
애플리케이션 노트
Introduction
Kevin Ashton first coined the phrase “The Internet of Things” in 1999 when discussing applications for RFID tags. From the simple tracking and counting of RFID objects, the Internet of Things has taken off with Machine-to-Machine (M2M), Big Data and Machine Learning, enabling applications such as the smart building, smart grid and intelligent transport systems.
IoT devices at the end nodes connect to the cloud or server for intelligence and analytics. Some connect directly and some via gateways, as shown in Figure 1. Gateways aggregate traffic from lower power networks onto higher capacity LANs and WANs. They typically include greater power supply and computing resources than end-nodes. Edge or fog applications running in gateways offload processing from both cloud and end-node sensors and actuators. End-nodes are often designed to have a long battery life, necessitating the efficient use of embedded computers and radio transmission. Intelligent threshold triggers in gateway applications make traffic more efficient by passing actionable information to central cloud servers. Gateways interface with the cloud and end-nodes via a heterogeneous mix of wireless technologies, both cellular and non-cellular. Radio interfaces address varying application needs depending on coverage, latency, throughput, energy efficiency, and cost.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
브라우저 쿠키가 만료되거나 브라우저 캐시가 지워지면 액세스 권한이 초기화됩니다. 콘텐츠에 다시 액세스 하시려면 다시 로그인하세요.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.