Choose a country or area to see content specific to your location
애플리케이션 노트
What is power conversion efficiency?
Efficiency is an assessment of how well time and effort are used to accomplish a specific task. If that task is the conversion of one form of power to another, the efficiency of the conversion indicates how well the power conversion is implemented. For an electrical power conversion process, efficiency is measured simply by dividing the output power in watts by the input power in watts and is expressed as a percentage. In power electronics, the Greek letter eta (η) is used to represent efficiency.
A perfect electrical power conversion process would have an efficiency of 100 percent. However, achieving 100 percent efficiency is not possible, because all real-life electronics lose some energy as heat. Some of the input power is used for the power conversion process itself, so that input power does not make it to the output. As a result, the efficiency must be less than 100 percent.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
브라우저 쿠키가 만료되거나 브라우저 캐시가 지워지면 액세스 권한이 초기화됩니다. 콘텐츠에 다시 액세스 하시려면 다시 로그인하세요.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.