Performing low-current measurements on printed circuit board assemblies (PCBAs) requires a precise low-current measurement instrument, such as a digital multimeter (DMM) or source measurement unit (SMU). These instruments must simultaneously measure voltage and current with high resolution and effective noise filtering. However, to conduct low leakage current testing during the in-circuit test stage, integrating an SMU into the in-circuit tester (ICT) is essential for achieving enhanced precision.
Integrating an SMU into the ICT requires establishing an interface and connecting the tester to the specific nodes on the device under test. Consequently, configuring the SMU involves setting output voltage, current parameters, and the desired measurement range. Test engineers also need test plans for both hardware and software test automation. Crafting a new test plan for each type of board ensures accurate testing.
Additional Resources for Low-Current Measurements on PCBAs
Need Help Finding the Right Solution for You?
What are you looking for?