Brochures
Microwave Measurement and Calibration
Keysight Technologies and ATE Systems
Accurate, reliable microwave measurement and automated calibration with multi-port fixturing.
In order to make accurate and reliable microwave measurements, test engineers have to bridge the gap between the high quality connectors on the front panel of their test instruments and the real-world interface on their device-under-test (DUT). The electrical interface of a DUT is rarely fitted with high-quality, traceable connectors and is likely to have a larger number of ports than the instrument has test connections.
In this environment, the connection between the instrument and the DUT will exhibit non-negligible losses, group delay and dispersion. To compensate for these degradations the test configuration must be calibrated, at the DUT ports, at least once per day. Manual calibration can be time-consuming, error-prone and reduces the overall throughput of the test system.
The solution is to automate the calibration procedures, but in a way that considers the test fixturing and the error correction to be applied. ATE Systems has developed a solution that allows automated calibration with minimum operator intervention. The solution can be used to establish reference planes right at the DUT, even when the interface is just a surface mount (SMT) pin.
Microwave Measurement and Calibration
The system can be used with Keysight Technologies’ PNA-L and PNA-X microwave network analyzers and PXA signal analyzer. It comprises an instrument correction module (ICM) that mounts directly onto the front panel of the analyzer and one or more fixture characterization modules (FCM) that connect to the DUT. The fixture characterization modules are connected to an FCM controller, which allows switching and multiplexing of instrument ports for multi-port applications.
The solution can be applied to S-parameter, scalar power, or noise measurements, allowing it to support any type of single or multi-function RF or microwave device. Software to control the system can be integrated into the network or signal analyzer.
The combination of ICM, FCMs and controller constitute a completely automated solution for in-situ calibration of single and multi-port devices. Once attached to the instrumentation, no calibration kit ever needs to be connected to the system to obtain error-corrected measurements. This means that the possibility of connecting the wrong standard or improperly torqueing a standard is eliminated. A system configured in this way provides measurements that are verified to TRL-level accuracy.
As an automated solution the potential for manual error is minimized. Calibration routines can be executed rapidly without the need to change hardware connections, allowing more frequent calibrations to be performed without compromising system availability.
ATE Systems’ solution when used with Keysight’s network and signal analyzers automates your calibration, allowing you to achieve accurate and reliable measurements on single and multi-port RF and microwave devices.
Können wir Ihnen behilflich sein?