N8480 Series Thermocouple Power Sensors

Technische Überblicke

The new Keysight Technologies, Inc. N8480 Series power sensors replace and surpass the legacy 8480 Series power sensors (excluding the D-model power sensors) in terms of its functionality and performance. A few of the key features offered are built-in Electrically Erasable Programmable Read-Only Memory (EEPROM), extended dynamic range, wider frequency range, and most important of all, higher accuracy and repeatability.

 Theory of Operation 

The new thermocouple Integrated Circuit (IC) is the major core improvement in the N8480 Series power sensors. The new IC not only inherits excellent linearity from the legacy 8480 power sensors but also extends the sensors’ dynamic range to –35 dBm, the lowest power measurement in the thermocouple power measurement solution. Figure 1 shows a basic power sensor block diagram for the thermocouple power-sensing elements. With reference to the block diagram, the new IC will convert any detected Radio Frequency (RF) power into a differential DC signal, and transmit the signal to the chopper circuit via a carefully designed differential path and layout. Then, a triggered 440 Hz power meter’s chopping signal is used to chop the DC signal into an AC signal. This process helps to decrease the electronic noise that occurs during the signal amplification, apart from the DC signal’s drift that enters the amplifier. The AC signal is amplified twice before it is transmitted to the power meter. The first stage amplifier is a differential instrumentation amplifier. It cancels the noise or thermocouple effect at the front end, thereby reducing the overall electronics noise floor by more than 50% compared to the legacy 8480 Series power sensors. The second stage amplifier is a conventional interface amplifier. It is used for signal amplification, as well as to match enable the power sensors with the Keysight power meters. The gain selection circuit is a new component added to the N8480 Series power sensors. This component optimizes the amplifier gain setting between the two stages of amplification and improves the power sensor’s performance in different dynamic ranges The thermistor in Figure 1 is the key element of the N8480 Series power sensors. It functions as a temperature sensing instrument as well as a feed indicator to the power meters during compensation. This computation is done by the connected power meter and it is used to minimize any sensor drift across the operating temperature range. The EEPROM serves as a register to store the calibration factors that carry the characteristics of a power sensor. The N8480 Series power sensors have been improved by optimizing algorithm structure functions to calculate the calibration factors and achieve better linearity and temperature compensation performance. The I2C buffer circuit and I2C remote I/O circuit function to control buses that transfer the data within the power sensor’s EEPROM and power meter. With all the improvement in the new thermocouple IC, electronic design, and introduction of a new correction algorithm, Keysight is now offering the power sensors with the widest dynamic range in the thermocouple measurement market. The N8480 Series power sensors provide better accuracy and power linearity compared to the legacy 8480 Series power sensors, in addition to the minimum measurement drift over temperature. These power sensors also offer easy start-up setting for RF power measurements. 

Why Choose the N8480 Series Power Sensors? 

Accurate power measurement 

The newly improved N8480 Series power sensors provide:

  • Wide dynamic range up to 55 dB 
  • Minimum power linearity performance of ± 0.52% 
  • Superior power measurement accuracy of less than 1% (with reference of 0 dBm at 50 MHz) 
  • More than 50% improvement in measurement repeatability.  
  • Convenient power measurement setting 

The N8480 Series power sensors have a built-in EEPROM, which allows the calibration factors to be loaded automatically to the power meter whenever the power sensors are connected to the power meter. 

Low cost with accurate power measurement 

The N8480 Series power sensors are affordable and a low-cost solution for accurate power measurement. Temperature-proof power measurement The N8480 Series power sensors are designed to be temperature sensitive. With the help of the optimized algorithm computation, the power measurement drift over temperature is minimized. 

N8480 Series Power Sensors in Today’s Wireless Signal Measurement 

Keysight is a leading innovator in the power sensors and power meters markets. One of its outstanding and recognizable products is the legacy 8480 Series power sensor, a thermocouple sensor technology introduced in the early 1970s. These power sensors can respond to the heat generated by the signal under test regardless of the type of signal. Hence, the new N8480 Series power sensors not only can measure the true average power for Continuous Waveform (CW) and true average signal, but can also measure complex modulated signals such as Music Local Area Network (mLAN), Worldwide Inter-operability for Microwave Access (WiMAX™), and even pulse signals — with better accuracy, repeatability, and reliability.