Technische Überblicke
Accuracy and peak performance are keys to competitive success in today’s lean factory environment. Your customers are asking for tighter tolerances and reduced costs. You want to control shop operations, reduce scrap, re-work, and improve productivity. Meeting these challenges means that you need to maximize the performance of your machine tools and, as a result, machine tool calibration has never been more important.
For more than four decades, Keysight technologies, Inc. Laser Calibration System have set the standard for laser-based metrology systems used to calibrate and verify machine tool and CMM accuracy. We introduced the laser calibration system and continue to offer robust performance.
Users benefit from improved process control and efficiency that help to optimize shop operations and reduce overall production cost. And, the powerful measurement capability of Keysight’s NIST traceable Laser Calibration System enables manufacturers to conform to key international standards. The Keysight 5530 Laser Calibration System is the ideal measurement tool to help manufacturers improve process control and efficiency for CMM and machine tool operations.
A powerful system that...
International standards
Verify Machine Performance and Improve Process Control
Customers continue to make demands on machine shops for more precise parts, manufactured to tighter specs. In order to maintain low inventories and trim cash flow, manufacturers want quick turnaround on parts. Short part runs, often using expensive materials, have become more common.
To help machine shops succeed in this increasingly competitive environment, Keysight designs and manufactures the 5530 Laser Calibration System with unmatched repeatability and reliability, making it the most cost-effective laser calibration system availabl
Machine tool manufacturers use the 5530 Laser Calibration System to:
The building blocks you need to improve process control and reduce costs allow you to:
When Should You Calibrate?
The 5530 Laser Calibration System helps you control quality and maximize productivity from the day your machine tool is delivered:
Acceptance testing
Machine tool manufacturers carefully test your equipment for accuracy before it leaves the factory, however equipment
often loses accuracy during shipment and installation. By calibrating with the 5530 Laser Calibration System, you prevent costly performance problems and ensure that your new investment begins paying its way immediately.
Scheduled calibration
Just as regular maintenance increases the life of your automobile, periodic calibration increases the life of your machine tool.
Keysight Technologies recommends that new machine tools be calibrated every six months during the first year-and-a-half of operation and then annually, unless calibration results warrant more frequent calibration. If environmental factors are extreme or if the machine tool is subjected to high stress or a crash, users should calibrate at shorter intervals.
Scheduled calibration with the 5530 provides a complete picture of your machine tool performance so that you can efficiently schedule workflow. You can schedule the most demanding work on the most accurate machines. And by identifying machines that cannot meet the accuracy requirements for a given job, the 5530 helps you control your processes, so you avoid costly scrap and schedule slips
Können wir Ihnen behilflich sein?