N7710C Fixed-Wavelength Laser Source

Datenblätter.

The Keysight N7710C Fixed-Wavelength Laser Source offers highly stable optical output power for use as a reference in calibration setups for handheld test equipment, or for generating a reference signal with the help of an optical modulator. Due to its Fabry-Pérot spectrum, the laser helps mitigate interference effects in the optical path, harnessing the reference power level against fluctuations that are common to test configurations using narrow-linewidth lasers.