An Enterprise Approach to Modernizing Test Automation Strategy

Case Studies

American Electric Power (AEP) is one of the largest energy companies in the US and powers millions of homes and businesses. Their electricity transmission network stretches more than 40,000 miles and is the largest in the country. Lead Automation Developer and Architect at AEP, John Alexander, was originally brought in as a consultant, having worked in testing automation across multiple sectors for two decades. His previous experience with Eggplant was instrumental in helping AEP improve automation and optimize DevOps.