SA8710A Automotive Cybersecurity Penetration Test Platform

Flyer

Test the resilience of your vehicle’s systems

The fully autonomous vehicle is the dream for most automakers and their customers around the world. To make this happen, the car needs to be connected to the outside world. These connections, however, expose the car to outside interference. Keysight can help you find vulnerabilities before anyone else does.

It’s a software problem

Cars run on software from various sources, and even the best coding practices have errors:

  • Software development policies differ even within a company. Consolidation andcoordination of code from suppliers is required.
  • There are 100,000,000 lines of code in a modern high-end car. With 0.1 coding errors per1000 lines of code, each car potentially has 10,000 software bugs.
  • A car’s typical lifespan is 10-15 years. It’s difficult for the suppliers to support the softwareover this long duration.

 Keysight can help

The Keysight Automotive Cybersecurity PEN test platform is a multi-layered solution to enable effective testing of your devices.

  • A combination of hardware, software and services to test the resilience of your ECUs,systems, or fully developed cars
    • Hardware that connects to the DUT via all relevant interfaces
    • Software that runs attacks against (exploits) the various interfaces
    • Subscription service for the Keysight threat library application and threatintelligence (ATI)
  • Validation of your systems using the Keysight threat databaseoReport any vulnerabilities and their severity
    • Make recommendations on how to address the vulnerabilities
  • Regression testing and enterprise level managementoSave the found vulnerabilities for repetitive use
    • Integrate with the Keysight Pathwave Lab Operations platform
  • Integration with customer’s enterprise platformoCloud and database services
    • Integrate your own tests