How to Validate BLE and WLAN IoT RF Performance

IoT Wireless Test
+ IoT Wireless Test

BLE and WLAN RF Performance Validation Workflow

IoT wireless performance depends on both sides of the radio link: how consistently a device transmits and how reliably it receives and responds. For Bluetooth® Low Energy and WLAN devices, RF performance validation helps engineers verify transmitter behavior, receiver performance, and signaling response before products move from development into manufacturing or deployment. This is especially important for compact IoT products that run final firmware, use small antennas, and may not support a physical RF test connector.

Keysight’s IoT wireless test solution supports conducted and non-conducted signaling tests for BLE and WLAN devices. Engineers can verify transmitter performance using measurements such as transmitter channel power, transmitter power envelope, and advertising interval. They can also characterize receiver behavior using channel-based packet error rate, composite packet error rate, and scan response data throughput measurements.

BLE and WLAN IoT RF Performance Test Solution

BLE and WLAN IoT devices must transmit within expected limits and reliably receive and respond to wireless signals. Keysight’s IoT wireless test solution supports conducted and non-conducted signaling tests on devices running final firmware, helping engineers verify transmitter channel power, transmitter power envelope, advertising interval, channel-based packet error rate, composite packet error rate, and scan response data throughput. These measurements help teams validate RF performance, establish test limits, identify marginal devices, and support repeatable R&D and manufacturing workflows. For over-the-air testing, shielded setups and path-loss awareness help preserve measurement confidence while keeping the focus on device performance.

See Block Diagram of BLE and WLAN IoT RF Performance Test Solution

BLE and WLAN IoT RF Performance Test Solution

Explore Products for BLE and WLAN IoT RF Performance Testing

Discover Resources and Insights

Additional Resources for BLE and WLAN IoT RF Performance Testing

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?