How to Test DC-DC Converter Efficiency

ATE DC Electronic Load
+ ATE DC Electronic Load

Measure DC-DC Conversion Efficiency

Testing DC-DC converter efficiency requires controlling the converter input voltage and output load while measuring electrical power at both sides of the device. The setup includes a programmable DC power source connected to the converter input and a programmable DC electronic load connected to its output. Voltage and current are measured at the input and output so that input power and output power can be determined at each operating point. The electronic load maintains a defined output load while the source establishes the required converter input conditions.

The efficiency measurement compares the power delivered by the converter with the power drawn from the input source. Conversion efficiency is calculated by dividing output power by input power as the input voltage is stepped through the required operating range. A settling interval between voltage steps allows the converter to reach a stable operating condition before voltage and current measurements are recorded. Repeating the measurement across the input range produces an efficiency profile that shows how conversion performance changes with input voltage under a controlled output load.

DC-DC Converter Efficiency Test Solution

Testing DC-DC converter efficiency requires controlling the electrical conditions at both sides of the converter and measuring the corresponding input and output power. The solution uses a programmable DC source to establish the converter input voltage and a Keysight ATE DC electronic load to apply a controlled load at the converter output. Voltage and current measurements are recorded at each operating point to determine input and output power and calculate conversion efficiency. The input voltage can be stepped through the required operating range while the output load remains controlled, allowing efficiency to be evaluated under repeatable conditions. This approach produces an efficiency profile across the converter operating range and supports automated characterization using consistent voltage, load, settling, and measurement conditions.

See Block Diagram of DC-DC Converter Efficiency Test Solution

See Block Diagram of DC-DC Converter Efficiency Test Solution

Explore Products for Our DC-DC Converter Efficiency Test Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?