Continuous Testing for DevOps and CI/CD

Validate complete user journeys across every platform with AI that adapts as your application changes.

Why Continuous Testing Matters

Why Continuous Testing Matters

Continuous testing automatically validates application changes at every stage of the CI/CD pipeline, from code commit through deployment. Tests trigger on every build, run in parallel across the full technology stack, and report results back to the development team without manual intervention.

The goal is to make quality validation a continuous, automated property of the delivery pipeline rather than a manual gate that blocks releases. Automation Intelligence (Eggplant Test) integrates into CI/CD pipelines through public APIs and standard toolchain connectors, triggering automated tests on every build without manual handoff.

Why Traditional Testing Falls Short for DevOps

DevOps teams can't ship fast if testing is a bottleneck. Manual gates and brittle automation defeat the point of continuous delivery.

Manual Testing Blocks Delivery

Manual quality gates introduce delays and inconsistency that interrupt CI/CD pipelines, defeating the speed continuous delivery is meant to enable.

Brittle Scripts Kill Pipelines

Tests that fail on every UI change cause pipeline failures, eroding trust and pushing teams to disable test stages entirely.

Tool Sprawl Breaks Visibility

Multiple testing tools across environments produce fragmented results, making it impossible to see overall pipeline health at a glance.

Coverage Gaps Surface Late

Without continuous testing across UI, API, and back-end layers, integration defects reach pre-production or worse, the user.

How Continuous Testing Works in Eggplant Test

Eggplant Test integrates directly into CI/CD pipelines, triggering AI-driven tests automatically and reporting results in formats DevOps teams can act on.

Where Continuous Testing Delivers the Most Value

  • DevOps teams shipping multiple times per day where manual quality gates would block release velocity 
  • Enterprise applications where every build needs to validate UI, API, and back-end behavior together
  • Regulated industries where every release needs an automated, auditable quality validation trail
  • Organizations replacing legacy test tooling that doesn't integrate cleanly with modern CI/CD pipelines
  • Teams scaling release frequency without scaling QA headcount 

 

Where Continuous Testing Delivers the Most Value

Common Questions About Continuous Testing

Testing that keeps pace with your releases.

Automated regression built into your pipeline. Run nightly, not just before a deadline.