Choose a country or area to see content specific to your location
What are you looking for?
Bridging design and physical testing to evaluate drop, impact, shock, and vibration compliance before hardware exists.
Unlock your free upgrade to the next bandwidth tier.
Strengthen 1.6T network reliability for AI-scale workloads from transceivers to interconnects.
Pair Keysight VSA software with the new XA5 signal analyzer for advanced visualization, demodulation, and analysis — start your 30-day trial today.
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
Get faster, clearer insights with our new multicore, 12-bit oscilloscope up to 33 GHz. Trade in your old oscilloscope and get credit toward a new XR8.
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
Keysight ZA2-class benchtop LCR meters include the E4980B Series
Keysight ZA2-class benchtop LCR meters include the E4980B Series which go far beyond fundamental impedance testing. They deliver highly precise and reliable measurements of passive components, supporting frequency ranges up to 3 GHz. Our benchtop LCR meters accurately measure a broad set of electrical parameters — including resistance, capacitance, inductance, and impedance — under a wide variety of test conditions, such as varying frequencies, signal levels, and bias voltages. Choose one of our popular configurations or configure one specific for your application. Need help selecting? Check out the resources below.
Highly accurate, repeatable measurements with basic accuracy as low as 0.05% ensure dependable characterization of passive components.
Includes robust open, short, and load compensation methods to minimize measurement errors caused by test fixtures, cable effects, and stray impedances.
Enables precise control over signal voltage and current to match the operating conditions of your DUT for evaluating nonlinear or sensitive components.
Features standard LAN, USB, and GPIB interfaces for remote control and seamless integration into automated test systems, making it ideal for high-throughput production lines.
Maximum frequency
1 MHz to 3 GHz
Target DUT
Capacitors, General-purpose device, Material
Type
Benchtop
E4981B
The capacitance meter E4981B offers a high speed with reliable capacitance measurements for ceramic capacitor testing in the production lines.
The Keysight Technologies, Inc. E4981B capacitance meter provides the best performance for ceramic capacitor manufacturing tests. Offering fast measurement speed and outstanding accuracy, the E4981B is the new standard in the industry.
Measurement Time
Basic Accuracy
More Features
A complete solution that replaces the 4268A, 4288A, and E4981A
The E4981B capacitance meter offers a high speed with reliable measurements for ceramic capacitor testing in the production lines. The E4981B realizes the measurement capabilities of capacitance from small to large values with accurate measurements. The E4981B capacitance meter contributes to improvements in the test throughput while attaining excellent component quality for ceramic capacitor testing.
E4980B
Keysight's E4980B precision LCR meter provides the best combination of accuracy, speed, and versatility for a wide range of component measurements.
The Keysight E4980B precision LCR meter combines accuracy, speed, and versatility for a wide range of component measurements. The E4980B is an essential tool for general R&D and manufacturing test of components and materials, offering fast measurement speed and performance at both low and high impedance ranges.
The versatile LAN, USB, and GPIB PC connectivity enhances your design and test productivity. For materials measurements, the E4980B paired with the Keysight N1500A-005/006 materials measurement suite simplifies the measurement process from fixture setup to report generation.
E4982A
The Keysight E4982A LCR meter provides the necessary performance when passive components are tested at high frequency.
Keysight E4982A LCR meter provides the best performance for the passive component manufacturing such as SMD inductors and EMI filters, where impedance testing at high frequencies is required. Not only for the manufacturing, E4982A can also be utilized for R&D, quality assurance with the powerful functions such as list measurements. By offering the unparalleled measurement speed and repeatability with excellent accuracy and impedance range, E4982A is the new standard for high speed component tests.
Innovate at speed with curated support plans and prioritized response and turn-around times.
Get predictable, lease-based subscriptions and full lifecycle management solutions—so you reach your business goals faster.
Experience elevated service as a KeysightCare subscriber to get committed technical response and more.
Ensure your test system performs to specification and meets local and global standards.
Make measurements quickly with in-house, instructor-led training, and eLearning.
Download Keysight software or update your software to the newest version.
LCR meters measure key parameters like impedance, capacitance, inductance, resistance, dissipation factor, and quality factor under defined frequency and voltage conditions. These parameters help determine how a component will perform in real-world circuits, especially over varying operating conditions. Parametric testing ensures that electronic components and systems perform as intended in real-world conditions, providing valuable data for design validation, quality assurance, and troubleshooting.
Parametric measurements are essential across various stages of the product lifecycle. During design, you can evaluate component parameters to verify that they meet the system specifications. In manufacturing, you can use LCR meters to ensure product quality and compliance. Once a system is deployed, LCR meters are used to verify functional behavior and diagnose performance degradation or damage.
Without precise measurements provided by LCR meters, designs would suffer from unchecked inefficiencies and risk catastrophic failure. Quantifying this opposition to electric current within materials or components accurately allows engineers to tailor designs for optimal performance.
Error compensation is important in an LCR meter because it ensures accurate and reliable measurements by correcting for systematic errors introduced by the test setup — especially those caused by cables, fixtures, and contact resistance.
When you're measuring small components, especially at higher frequencies, even minor sources of error like stray capacitance, lead inductance, or parasitic resistance from the test leads can significantly distort the actual measurement. These errors can make a capacitor look like it has more inductance than it should, or make an inductor appear to have more resistance.
By performing compensation, the LCR meter essentially “zeroes out” the influence of the test environment so that only the true characteristics of the device under test (DUT) are measured. This is especially critical in applications requiring high precision or where components have very small values, such as in RF, medical, or aerospace electronics.
For integration into a high-throughput production line, an LCR meter must deliver a combination of speed, accuracy, and seamless automation support. Fast measurement speed is essential to keep pace with rapid test cycles. High accuracy and repeatability are equally important to ensure consistent quality control, especially when testing to tight tolerances. Automation is another critical requirement. LCR meters used in production should support remote control capabilities via standard interfaces like USB, LAN, and GPIB. Support for reliable test fixtures is also essential for minimizing lead resistance and maximizing measurement precision. Additionally, open/short/load compensation is required to remove the effects of cables and fixtures from the measurement, ensuring accurate results across multiple stations or setups.