Keysight Oscilloscope Glossary
What is a Mixed-Signal Oscilloscope?
Introduction
It might surprise you to learn that a single piece of test equipment can provide invaluable insight into both the analog and digital aspects of an electronic circuit. This versatile device is the mixed-signal oscilloscope (MSO).
Perfectly marrying the functionality of digital storage oscilloscopes (DSO) and logic analyzers, MSOs have revolutionized the way engineers approach complex system design and troubleshooting.
In the following sections, we will delve deep into what an MSO is, how it works, and its practical applications, with a detailed comparative table for added clarity.
Buy Oscilloscopes at a Great Discount
Features of a Mixed-Signal Oscilloscope (MSO)
A mixed-signal oscilloscope combines the functionality of a digital oscilloscope, which captures analog signals, with a logic analyzer that detects digital signals. This means it can display and analyze analog and digital signals simultaneously, providing a comprehensive perspective of how these signals interact in the system under test.
The key features of an MSO include:
- Analog channels: These are akin to the input channels found in regular oscilloscopes. They allow engineers to observe, analyze, and compare multiple analog waveforms simultaneously.
- Digital channels: The digital channels serve a similar purpose as those on a logic analyzer. They allow the observation and analysis of multiple digital signals concurrently.
- Time correlation: Perhaps the most powerful feature of an MSO is the ability to view analog and digital signals together on the same timeline. This time-correlation feature provides a holistic view of the system under test.
Key Takeaway
Mixed-Signal Oscilloscopes (MSOs) offer an unparalleled view into the complex interactions between digital and analog signals in modern electronic systems, making them an indispensable tool for efficient design validation, troubleshooting, and optimization. By understanding the right selection parameters and leveraging advanced features, engineers can harness the full potential of MSOs for their specific applications.
The Working Principle of a Mixed-Signal Oscilloscope
Understanding the working principle of an MSO is crucial for its effective utilization. Let's break it down.
1. Input Stage
The MSO's journey begins with the input stage. Here, the signals from the device under test (DUT) are fed into the oscilloscope via the analog and digital channels.
2. Signal Conditioning
Next, the incoming signals undergo signal conditioning, where they are amplified, filtered, or attenuated as necessary to optimize them for accurate viewing and measurement.
3. Analog-to-Digital Conversion
The conditioned analog signals are then converted to digital format through an Analog-to-Digital Converter (ADC). Digital signals bypass this stage as they're already in the required format.
4. Digital Signal Processing and Display
Post conversion, all signals (analog-turned-digital and digital) are processed using sophisticated digital signal processing algorithms. The processed signals are then displayed on the MSO's screen, showing analog waveforms and digital data concurrently. The results can be visualized in various forms, including eye diagrams, histograms, and FFT plots, among others.
Practical Applications of MSOs
Mixed-signal oscilloscopes have become an indispensable tool in many areas, given their versatility and capabilities.
- Debugging complex circuits: In complex digital systems where analog and digital signals interact, MSOs are invaluable in debugging. The MSO’s ability to correlate digital activities with analog phenomena in real time is critical to understanding system behavior.
- Embedded systems: MSOs are often used to verify and debug timing issues, hardware-software integration, and other challenges in embedded systems.
- Automotive electronics: With the increasing incorporation of electronics in automotive systems, MSOs are used to analyze the interaction between digital control signals and analog sensor and actuator signals.
- Power electronics: MSOs are used for characterizing power devices, assessing performance, and identifying issues in power supply design, especially when the operation involves digital control signals.
- Internet of things(IoT): IoT devices typically combine analog and digital systems. MSOs help debug and validate design for IoT devices.
Comparative Overview: MSO vs. DSO vs. Logic Analyzer
| Features | Mixed-Signal Oscilloscope (MSO) | Digital Storage Oscilloscope (DSO) | Logic Analyzer |
|---|---|---|---|
| Analog Channels | Yes | Yes | No |
| Digital Channels | Yes | No | Yes |
| Time Correlation | Yes | No | No |
| High-Speed Timing Analysis | Yes | No | Yes |
| Detailed Analog Waveform Analysis | Yes | Yes | No |
| Complex Triggering Capabilities | Yes | Yes | Yes |
Yes
Yes
No
Yes
No
Yes
Yes
No
No
Yes
No
Yes
Yes
Yes
No
Yes
Yes
Yes
How to Choose a Mixed-Signal Oscilloscope
Choosing the right mixed-signal oscilloscope (MSO) is crucial to effectively analyzing the interaction of analog and digital signals in a system. With the wide range of options available in the market, this task might seem daunting.
Understanding key parameters such as bandwidth, sample rate, channel count, and probe compatibility can guide you towards making an informed decision.
Bandwidth
Bandwidth is perhaps the most critical parameter when selecting an MSO. It defines the frequency range that the oscilloscope can accurately measure. To capture the fastest signal component in your system, choose an oscilloscope with a bandwidth five times higher than the maximum signal frequency. This rule of thumb allows the oscilloscope to capture up to the fifth harmonic, providing an accurate representation of your signal
Sample Rate
The sample rate is another vital parameter, directly impacting the accuracy of waveform representation. As per the Nyquist theorem, the sample rate should be at least twice the maximum frequency component of the signal. However, to capture higher frequency harmonics and accurately reproduce signal shapes, a sampling rate greater than twice the bandwidth is recommended.
Channel Count
The number of channels on an oscilloscope defines how many signals it can observe concurrently. A higher channel count allows for better understanding of complex systems where multiple analog and digital signals interact.
When choosing the channel count, consider both analog and digital channels. For mixed-signal analysis, you may require multiple channels to monitor several analog and digital lines simultaneously.
Probe Compatibility
Probes serve as the interface between the device under test (DUT) and the oscilloscope. The probe's specifications should match or exceed the oscilloscope's performance to ensure measurement accuracy. When choosing an MSO, consider what types of probes it supports, such as passive probes, active voltage probes, or current probes. Ensure that the probes are suited for the type of measurements you intend to make.
Other Parameters to Consider
- Memory depth: This is the total number of samples that the oscilloscope can store. A greater memory depth allows the oscilloscope to capture a longer time period at the maximum sample rate.
- Waveform update rate: This indicates how quickly the oscilloscope processes and displays waveforms. A higher update rate ensures a more responsive oscilloscope and better chance to capture random and infrequent events.
- User interface and software: Evaluate the user-friendliness of the oscilloscope’s interface and software. Features like touch screen, automated measurements, and decoding capabilities can save a significant amount of time and make it easier to use.
Advanced Features and Capabilities of Modern MSOs
Modern mixed-signal oscilloscopes (MSOs) offer a plethora of advanced features that go beyond simple waveform visualization, providing deeper insight into your system's operation.
Let's delve into some of these features, which include advanced triggering, automated measurement capabilities, protocol decoding, and waveform math functions.
Advanced Triggering
In complex electronic systems, specific events often provide crucial insights into system behavior. Advanced triggering allows you to isolate these events from a sea of signal activity, thereby providing valuable troubleshooting capability.
MSOs provide a wide range of triggering options. Edge and pulse width triggers are common, but modern oscilloscopes go beyond these. For instance, runt trigger can capture pulses that fall below or exceed specified amplitude limits. Window trigger can isolate events that either enter or exit a defined voltage and time window.
Modern MSOs offer protocol-specific triggering for I2C, SPI, UART, and other common bus systems, allowing engineers to home in on specific data packets, addresses, or error conditions.
Automated Measurement Capabilities
Modern MSOs are equipped with automated measurement capabilities that simplify the analysis process. With a push of a button, you can measure parameters such as rise time, fall time, frequency, period, peak-to-peak voltage, RMS voltage, and many others.
These measurements are often complemented by statistical information like mean, min/max, and standard deviation, providing a comprehensive understanding of signal behavior over time.
Protocol Decoding
With the increasing use of serial buses in electronic systems, the ability to decode and analyze protocol-based communication has become essential. Modern MSOs offer built-in decoders for popular protocols such as I2C, SPI, CAN, LIN, and more. These decoders translate the raw bitstream into human-readable format (bytes, packets, frames), allowing engineers to debug their system at the protocol level.
Some oscilloscopes also offer event tables, which link decoded information directly to the waveform, and search functions, which enable users to find specific events within the decoded data.
Waveform Math Functions
The ability to perform mathematical operations on waveforms is a powerful feature found in modern MSOs. Basic operations include addition, subtraction, multiplication, and division between channels. More advanced functions include integration, differentiation, FFT (Fast Fourier Transform) for frequency domain analysis, and user-defined expressions.
Additionally, digital filtering allows engineers to isolate the portion of the signal of interest, enhancing measurement accuracy. Waveform math functionality can be invaluable in characterizing system response, exploring signal relationships, and conducting advanced analysis.
Conclusion
Mixed-signal oscilloscopes have truly become the Swiss Army Knife for modern engineers. By providing comprehensive and simultaneous analysis of both analog and digital signals, they're integral to understanding the complex interactions in today's electronic systems.
To streamline system design, testing, and debugging processes, it is crucial to select the appropriate MSO based on parameters like bandwidth, sample rate, channel count, and probe compatibility. By utilizing its advanced features such as triggering, automated measurement, protocol decoding, and waveform math functions, you can optimize your workflow and achieve more efficient results.
As an engineer or technician in the realm of electronics, investing in an MSO becomes a necessity rather than a luxury. If you are looking for the best premium used test equipment, check out Keysight's Used Equipment Store, a trusted source for premium used oscilloscopes.
You'll find a wide variety of high-quality, refurbished oscilloscopes, including advanced mixed-signal oscilloscopes, signal analyzers, network analyzers and more, all of which are thoroughly tested and certified by Keysight.
Visit Keysight's Used Equipment Store today, and find the perfect oscilloscope that meets your needs and budget!
Browse Oscilloscopes at a Great Discount
最多可以选择3台仪器进行对比
Whenever You’re Ready, Here Are
5 Ways We Can Help You
Browse our Premium Used Oscilloscopes.
Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
Contact our sales support team
Create an account to get price alerts and access to exclusive waitlists
Talk to your account manager about your specific needs