mmWave 5G Non-Signaling Solution

Solution Briefs

Streamlined testing across any 3GPP mmWave band

 

Mobile operators around the world are accelerating 5G deployments to capture early market opportunities. As a result, wireless equipment manufacturers need to support a more rapid pace of development while addressing evolving 5G New Radio (NR) specifications set by 3GPP and other standards developing organizations (SDOs). The introduction of enhanced Mobile Broadband (eMBB) services and vertical applications means next generation mobile devices need to support an increasing number of millimeter-wave (mmWave) frequency bands.

 

Most 5G mobile devices operating in mmWave frequency spectrum rely on modules with highly integrated RFIC architectures. This requires new 5G designs to be verified across both intermediate frequencies (IF) and mmWave frequencies. Since 5G mmWave devices use phased-array antennas that lack connectorized ports, performance validation needs to take place in Over-the-Air (OTA) test environments. Creating and maintaining a calibrated system when using multiple platforms to perform measurements in OTA test environments can be challenging and lead to unreliable measurement results.