5G Protocol R&D Toolset

Solution Briefs

The Fastest Path to 5G

5G is rapidly approaching. Mobile operators are fast-tracking their 5G deployment plans, leading to the need for chipset and device manufacturers to accelerate their development activities. 5G brings new and powerful capabilities to support use cases that require much faster data rates, ultra-reliable low-latency as well as that enable massive machine-type communications. Delivering these use cases with the desired communications system performance requires technologies that operate at mm-Wave frequencies using wider bandwidths, as well as beamforming techniques. In other words, 5G produces significant challenges that the device ecosystem needs to address quickly and accurately when prototyping new designs.