E18-3dwq1
CVSS:
7.5 CVSS:3.0/AV:N/AC:H/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2017
Description
This strike exploits a vulnerability in the Microsoft Edge browser. Specifically, the vulnerability exists in the javascript Chakra engine. It is possible to create javascript in such a way that allows for the scriptFunction to be exposed to the user as 'this' when getting the length property. When this happens type confusion occurs. This may lead to a denial of service condition in the browser, or potentially remote code execution.
CVE
https://code.google.com/p/google-security-research/issues/detail?id=1403