Clipbucket Arbitrary PHP Code Execution

Strike ID:
E17-mggs1
CVSS:
7.5 (AV:N/AC:L/Au:N/C:P/I:P/A:P)
False Positive:
f
Variants:
2
Year:
2017

Description

This strike exploits a file upload vulnerability in Clipbucket web application. The vulnerability is due to improper validation of the user controlled input to the file uploading scripts. By exploiting this vulnerability, a remote, unauthenticated attacker can upload any file including PHP scripts and execute them on the target server. NOTE: When run in one-arm mode, target web application index needs to be available at http://[server].

References